<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: DSP56720 Boot SPI EEPROM</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1885029#M23073</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I attach the two files for DSP5672x, hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jun 2024 09:33:49 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-06-11T09:33:49Z</dc:date>
    <item>
      <title>DSP56720 Boot SPI EEPROM</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1880089#M22934</link>
      <description>&lt;P&gt;I am wondering if anybody knows what pin /CS should be coming from for a boot SPI EEPROM for the DSP56720? I know this is an older DSP but I have a handful of trays of them I'm trying to use up for a some low-volume DSP products. A bootloader listing would be fine, too, I can read the code pretty easily. Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 22:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1880089#M22934</guid>
      <dc:creator>daleulan2</dc:creator>
      <dc:date>2024-06-03T22:20:55Z</dc:date>
    </item>
    <item>
      <title>Re: DSP56720 Boot SPI EEPROM</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1885029#M23073</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I attach the two files for DSP5672x, hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jun 2024 09:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1885029#M23073</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-06-11T09:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: DSP56720 Boot SPI EEPROM</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1886441#M23103</link>
      <description>&lt;P&gt;Yes, this is perfect. I can hook the EEPROM up based on this and get my PCBs made. I am booting from serial EEPROM in an 8-pin DIP socket initially, then I have a SMD flash on the external data bus as well as a few megabytes of SRAM for delay. I should be able to boot from either the soldered-down parallel flash or the serial EEPROM.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 23:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/DSP56720-Boot-SPI-EEPROM/m-p/1886441#M23103</guid>
      <dc:creator>daleulan2</dc:creator>
      <dc:date>2024-06-12T23:52:44Z</dc:date>
    </item>
  </channel>
</rss>