<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: PN532 pin RSTOUT_N</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1880300#M22943</link>
    <description>&lt;P&gt;Yes, I think it's pin 38 I'm referring to, as you can see from the png image, which I attached to the first post.&lt;BR /&gt;I must have gotten the pin numbering wrong.&lt;/P&gt;&lt;P&gt;so can I ground it directly?&lt;BR /&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Tue, 04 Jun 2024 05:16:19 GMT</pubDate>
    <dc:creator>frank55</dc:creator>
    <dc:date>2024-06-04T05:16:19Z</dc:date>
    <item>
      <title>PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1874526#M22792</link>
      <description>&lt;P&gt;I connected the RSTPON pin (26) to ground via a BJT (BC547B npn) driven by an Arduino pin. I would like to know if I can leave this pin connected to ground for an indefinite time (for example a month) without creating problems.&lt;/P&gt;&lt;P&gt;PN532 pcb&lt;/P&gt;&lt;P&gt;&lt;A title="object pn532" href="http://osoyoo.com/2017/07/19/pn532-nfc-rfid-module-for-arduino/" target="_self"&gt;http://osoyoo.com/2017/07/19/pn532-nfc-rfid-module-for-arduino/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;pin of reference&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 09:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1874526#M22792</guid>
      <dc:creator>frank55</dc:creator>
      <dc:date>2024-05-24T09:47:58Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1875740#M22818</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234067"&gt;@frank55&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please, consider that &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-integrated-solution:PN5321A3HN" target="_blank"&gt;PN532&lt;/A&gt; is Not Recommended for New Designs and our support for this device may be limited. For new designs, we recommend using&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-plug-and-play-controller-with-integrated-firmware-and-nci-interface:PN7160" target="_blank"&gt;PN7160&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;From the &lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/PN532_C1.pdf" target="_blank"&gt;PN532 Data Sheet&lt;/A&gt;, Chapter 7 Pinning information, pin 26 corresponds to RSTOUT_N, which is an output pin used to indicate the reset status. However, since it seems that this product is from a third-party, I will recommend you contacting the manufacturer for further support on this part.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 20:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1875740#M22818</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-05-27T20:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1879237#M22900</link>
      <description>&lt;P&gt;but on aliexpress it is the cheapest version, for a hobbyist like me.&lt;BR /&gt;I also saw a schematic from adafruit that the same pin is connected to vpp via a 10k resistor.&lt;BR /&gt;why if it's only outgoing?&lt;/P&gt;&lt;P&gt;&lt;A href="https://learn.adafruit.com/assets/26820" target="_self"&gt;https://learn.adafruit.com/assets/26820&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 01 Jun 2024 12:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1879237#M22900</guid>
      <dc:creator>frank55</dc:creator>
      <dc:date>2024-06-01T12:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1879995#M22929</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think you are referring to Pin 38 - RSTPD_N, is this correct? If so, this input pin is active low; when this pin is set to logic 0, the PN532 goes into Hard Power Down (HPD) mode. The PN532 goes into reset and the RSTOUT_N signal is driven low.&lt;/P&gt;
&lt;P&gt;For more information on this, please refer to &lt;A href="https://www.nxp.com/docs/en/nxp/data-sheets/PN532_C1.pdf" target="_blank"&gt;PN532 Data Sheet&lt;/A&gt;, Section 8.5.2 Reset modes and Section 8.5.5 Low power modes.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 17:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1879995#M22929</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-06-03T17:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1880300#M22943</link>
      <description>&lt;P&gt;Yes, I think it's pin 38 I'm referring to, as you can see from the png image, which I attached to the first post.&lt;BR /&gt;I must have gotten the pin numbering wrong.&lt;/P&gt;&lt;P&gt;so can I ground it directly?&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jun 2024 05:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1880300#M22943</guid>
      <dc:creator>frank55</dc:creator>
      <dc:date>2024-06-04T05:16:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 pin RSTOUT_N</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1880790#M22958</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You could set this pin to 0 to put the device into Hard Power Down mode as described in Section 8.5.5.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jun 2024 16:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532-pin-RSTOUT-N/m-p/1880790#M22958</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-06-04T16:26:48Z</dc:date>
    </item>
  </channel>
</rss>