<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PTP Sync message not sent in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PTP-Sync-message-not-sent/m-p/1871746#M22766</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;I'm having a problem with the usage of KSZ8567 switch in our System-On-Module which uses i.MX 6ULL processor. The PTP Sync messages are being dropped and I can only see malformed follow-up messages on wireshark. Therefore, I'm not able to synchronize the time between the master and slave component (Here, Our System-On-Module act as master with KSZ8567 switch and another board is connected to it as slave). I also tried to implement the workaround suggested by KSZ8567 errata data sheet (Module 17: PTP messages get dropped in PTP 2-Step Mode) but still it doesn't work. There is a feature called Tail Tagging in the driver implementation. When I disable this feature, I'm able to see the sync messages but then the switch stops functioning and I can't detect the slave component.&lt;/P&gt;&lt;P&gt;Could you please provide appropriate solution for it?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Sahil Mittal&lt;/P&gt;</description>
    <pubDate>Thu, 23 May 2024 07:43:06 GMT</pubDate>
    <dc:creator>EmbeddedEngineer</dc:creator>
    <dc:date>2024-05-23T07:43:06Z</dc:date>
    <item>
      <title>PTP Sync message not sent</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PTP-Sync-message-not-sent/m-p/1871746#M22766</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;I'm having a problem with the usage of KSZ8567 switch in our System-On-Module which uses i.MX 6ULL processor. The PTP Sync messages are being dropped and I can only see malformed follow-up messages on wireshark. Therefore, I'm not able to synchronize the time between the master and slave component (Here, Our System-On-Module act as master with KSZ8567 switch and another board is connected to it as slave). I also tried to implement the workaround suggested by KSZ8567 errata data sheet (Module 17: PTP messages get dropped in PTP 2-Step Mode) but still it doesn't work. There is a feature called Tail Tagging in the driver implementation. When I disable this feature, I'm able to see the sync messages but then the switch stops functioning and I can't detect the slave component.&lt;/P&gt;&lt;P&gt;Could you please provide appropriate solution for it?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Sahil Mittal&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 07:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PTP-Sync-message-not-sent/m-p/1871746#M22766</guid>
      <dc:creator>EmbeddedEngineer</dc:creator>
      <dc:date>2024-05-23T07:43:06Z</dc:date>
    </item>
  </channel>
</rss>