<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7642, LPUART examples not working in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1867980#M22677</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problems with lpuart poll/interrupt examples on devkit OM27642EVK.&amp;nbsp;PN7642 SDK 2.12.5.&lt;/P&gt;&lt;P&gt;There is a wait inside LPUART_Init() which makes the mcu reset over and over:&lt;BR /&gt;PN76_Common_Wait(50);&lt;BR /&gt;I tried removing this wait and added a for loop instead. Then, there is no reset but I only see some junk on putty when it tries to write the app starting msg. And if I type in putty to get an echo,&amp;nbsp;LPUART_PollReceive fails.&lt;/P&gt;&lt;P&gt;I have set the jumpers/switches according to the readme and I use ftdi cable and putty to send/receive uart packets. Is there any common/obvious mistake in my setup?&lt;BR /&gt;Why should PN76_Common_Wait() fail? Can I just replace it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 May 2024 10:31:39 GMT</pubDate>
    <dc:creator>Parmiss</dc:creator>
    <dc:date>2024-05-17T10:31:39Z</dc:date>
    <item>
      <title>PN7642, LPUART examples not working</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1867980#M22677</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have problems with lpuart poll/interrupt examples on devkit OM27642EVK.&amp;nbsp;PN7642 SDK 2.12.5.&lt;/P&gt;&lt;P&gt;There is a wait inside LPUART_Init() which makes the mcu reset over and over:&lt;BR /&gt;PN76_Common_Wait(50);&lt;BR /&gt;I tried removing this wait and added a for loop instead. Then, there is no reset but I only see some junk on putty when it tries to write the app starting msg. And if I type in putty to get an echo,&amp;nbsp;LPUART_PollReceive fails.&lt;/P&gt;&lt;P&gt;I have set the jumpers/switches according to the readme and I use ftdi cable and putty to send/receive uart packets. Is there any common/obvious mistake in my setup?&lt;BR /&gt;Why should PN76_Common_Wait() fail? Can I just replace it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 10:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1867980#M22677</guid>
      <dc:creator>Parmiss</dc:creator>
      <dc:date>2024-05-17T10:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642, LPUART examples not working</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1949419#M25401</link>
      <description>&lt;P&gt;I know this problem is fixed;&amp;nbsp; it is happened on the PN7642 previous versions , the possible solution is to update the software of the PN7642 , the latest version can be found at the installation folder of cockpit. Or you can run demo pnev7642fama_check_nxpfw_update to update firmware to the latest version.&lt;/P&gt;
&lt;P&gt;If you can not update the binary in mass storage mode, please refer to below thread.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786251" target="_blank"&gt;Solved: PN7642 Mass Storage Device Activation - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In case other customers are having the same issue, I hope this can help.&lt;/P&gt;</description>
      <pubDate>Sat, 07 Sep 2024 12:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1949419#M25401</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-09-07T12:57:10Z</dc:date>
    </item>
  </channel>
</rss>