<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: NXP LIN Bus Transceivers Configure Commander/Responder</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1858379#M22474</link>
    <description>&lt;P&gt;I am still confused with whether SJA1124 can be used as a slave or not.&lt;/P&gt;
&lt;P&gt;We tried by programming MCFG bits to 00(i.e. terminated with Responder), but still not able to receive data which master is sending&lt;/P&gt;</description>
    <pubDate>Thu, 02 May 2024 11:16:41 GMT</pubDate>
    <dc:creator>nxf33425</dc:creator>
    <dc:date>2024-05-02T11:16:41Z</dc:date>
    <item>
      <title>NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1597583#M16674</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&lt;SPAN&gt;I am looking into purchasing some LIN Bus&amp;nbsp;transceivers such as the NXP&amp;nbsp;TJA1124 or SJA1124 series. However after reading through the data sheet I am a bit confused about configuring the&amp;nbsp;transceiver as a commander or responder.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Referencing&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Section 3 In this data sheet&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/SJA1124DS.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/data-sheet/SJA1124DS.pdf&lt;/A&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;BLOCKQUOTE&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;[1] &amp;nbsp;The SJA1124A LIN commander termination is SPI-configurable and consists of a diode and a pull-up resistor of 900 Ω to 1100 Ω, as specified in LIN 2.x, ISO 17987-4:2016 (12 V LIN) and SAE J2602-1.&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;[2] &amp;nbsp;The SJA1124B LIN commander termination is fixed and consists of a diode and a pull-up resistor of 900 Ω to 1010 Ω.&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;Does this mean that it can be configured via SPI for&amp;nbsp;SJA1124A but not&amp;nbsp;SJA1124B?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Or that SJA1124A can be&amp;nbsp;commander or responder but SJA1124B can only be a commander?&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So is this chip configurable as a commander/responder if so is the termination internal or do extra&amp;nbsp;components need to be added to the board?&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 10 Feb 2023 20:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1597583#M16674</guid>
      <dc:creator>TheMDev</dc:creator>
      <dc:date>2023-02-10T20:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1597834#M16681</link>
      <description>&lt;P&gt;Please read datasheet page 15 for more detail explain--&lt;/P&gt;
&lt;P&gt;The SJA1124A contains Multiple Time Programmable (MTP) non-volatile memory (NVM)&lt;BR /&gt;cells that allow the default configuration of the LIN commander pull-up to be programmed&lt;BR /&gt;(the NVM registers are read-only in the SJA1124B).&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 05:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1597834#M16681</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-02-13T05:19:40Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1598355#M16696</link>
      <description>&lt;P&gt;Hi, thank you for your response and clarifying the difference between the&amp;nbsp;&lt;SPAN&gt;SJA1124A/&lt;/SPAN&gt;&lt;SPAN&gt;SJA1124B. However, referencing&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Table 1 and&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Table 12, I am still unclear if the&amp;nbsp;&lt;SPAN&gt;SJA1124A can be configured as a commander and responder. The note under table one lists that the pull-up resistor is approximately 1k. Referencing table 12, it only allows the configuration of the 1k resistor for different power states. However, to my knowledge, responder nodes are typically terminated with a 30k pull-up. So can the&amp;nbsp;SJA1124A be configured as a responder with an external 30k pull-up, or is it only able to be a commander?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 19:19:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1598355#M16696</guid>
      <dc:creator>TheMDev</dc:creator>
      <dc:date>2023-02-13T19:19:44Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1598670#M16704</link>
      <description>&lt;P&gt;Hi :&lt;/P&gt;
&lt;P&gt;The LINx pins of the xJA1124 are equal. A LIN slave pull-up Rslave and LIN master pull-up&lt;BR /&gt;Rmaster, each in series with a reverse current protection diode, are internally connected to&lt;BR /&gt;pin BAT. The LIN master pull-up Rmaster can be disabled in case of detected faults, e.g.&lt;BR /&gt;short-circuit between LIN and ground. In the SJA1124A, the LIN master pull-up&lt;BR /&gt;termination can be programmed per channel via the MCFG register (refer to section&lt;BR /&gt;“Programming of MTPNVM” in the data sheet [1]. Note: The number of programming&lt;BR /&gt;cycles should not exceed 63 (3Fh). This could lead to malfunction of the device.&lt;/P&gt;
&lt;P&gt;The specified range of Rmaster [1][2] for the variants SJA1124A, TJA1124A and TJA1124B&lt;BR /&gt;differs from the variants SJA1124B and TJA1124C. As illustrated in Fig 3, latter variants,SJA1124B and TJA1124C, have a lower maximum value whereas the minimum value is&lt;BR /&gt;unchanged.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_0-1676359749156.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/210801i9EC46B6B8CB7E4FF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_0-1676359749156.png" alt="guoweisun_0-1676359749156.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_0-1676359749156.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With this lower Rmaster maximum value, the maximum RC time constant of the LIN&lt;BR /&gt;network can be reduced. This enables the use of an integrated LIN master pull-up in LIN&lt;BR /&gt;networks, which are designed based on an external LIN master pull-up with 1 kΩ ±1%.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 07:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1598670#M16704</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-02-14T07:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1740449#M19677</link>
      <description>&lt;P&gt;Hi, for me it is not clear if&amp;nbsp;&lt;SPAN&gt;SJA1124A/&lt;/SPAN&gt;&lt;SPAN&gt;SJA1124B is able to works as a responder?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 13:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1740449#M19677</guid>
      <dc:creator>christoph_bierwipfl</dc:creator>
      <dc:date>2023-10-16T13:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1858379#M22474</link>
      <description>&lt;P&gt;I am still confused with whether SJA1124 can be used as a slave or not.&lt;/P&gt;
&lt;P&gt;We tried by programming MCFG bits to 00(i.e. terminated with Responder), but still not able to receive data which master is sending&lt;/P&gt;</description>
      <pubDate>Thu, 02 May 2024 11:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/1858379#M22474</guid>
      <dc:creator>nxf33425</dc:creator>
      <dc:date>2024-05-02T11:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: NXP LIN Bus Transceivers Configure Commander/Responder</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/2091463#M28524</link>
      <description>Changing the pullup fuse:&lt;BR /&gt;reg 0x10 = 0x80 to disable sleeping&lt;BR /&gt;reg 0xf0-f2 reads 0xAA 0x40 0x00&lt;BR /&gt;0xf0 = 0&lt;BR /&gt;0xf2 = 0xA1&lt;BR /&gt;Wait at least 1 second after setting the crc</description>
      <pubDate>Mon, 05 May 2025 13:30:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-LIN-Bus-Transceivers-Configure-Commander-Responder/m-p/2091463#M28524</guid>
      <dc:creator>Rikus</dc:creator>
      <dc:date>2025-05-05T13:30:38Z</dc:date>
    </item>
  </channel>
</rss>