<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can we stop the timers when debugging? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Can-we-stop-the-timers-when-debugging/m-p/1850224#M22253</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP support.&lt;/P&gt;
&lt;P&gt;We do not have specifically a debugger option for the RTC debugging as you mention what we can do in this case is or either&amp;nbsp; use an RTC interrupt and do an RTC stop and re-start the RTC once the interruption is gone.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Apr 2024 22:26:55 GMT</pubDate>
    <dc:creator>nxf77486</dc:creator>
    <dc:date>2024-04-18T22:26:55Z</dc:date>
    <item>
      <title>Can we stop the timers when debugging?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Can-we-stop-the-timers-when-debugging/m-p/1849860#M22243</link>
      <description>&lt;P&gt;Processor K32W041, but most likely applicable to all ARM Cortex-M4&lt;/P&gt;&lt;P&gt;How can I stop the timer peripherals when stopped at a breakpoint?&lt;/P&gt;&lt;P&gt;When debugging my code, the processor stops at a breakpoint but the Real Time Clock (RTC) continues. This creates problems since the RTC is used for timeouts and interrupt driven timers. Is there a mechanism where I can specify which timers should stop on entering the debug state? Something like the 'DBGMCU Peripheral Freeze registers' in the STM32MP157 or STM32WBA5xxx?&lt;/P&gt;&lt;P&gt;Alternatively, is there a method to test whether the debugger is in a stopped state? So, when entering the timer interrupt routine, I could test for this debugger state and then ignore the interrupt.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 12:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Can-we-stop-the-timers-when-debugging/m-p/1849860#M22243</guid>
      <dc:creator>ckielstra</dc:creator>
      <dc:date>2024-04-18T12:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: Can we stop the timers when debugging?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Can-we-stop-the-timers-when-debugging/m-p/1850224#M22253</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP support.&lt;/P&gt;
&lt;P&gt;We do not have specifically a debugger option for the RTC debugging as you mention what we can do in this case is or either&amp;nbsp; use an RTC interrupt and do an RTC stop and re-start the RTC once the interruption is gone.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Apr 2024 22:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Can-we-stop-the-timers-when-debugging/m-p/1850224#M22253</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-04-18T22:26:55Z</dc:date>
    </item>
  </channel>
</rss>