<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic requesting for isolated CAN controller IC in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/requesting-for-isolated-CAN-controller-IC/m-p/1848073#M22201</link>
    <description>&lt;P&gt;Hi Good Afternoon&lt;BR /&gt;&lt;BR /&gt;Can you suggest the Isolated CAN controller IC's , part number for the below requirements mentioned&lt;/P&gt;&lt;P&gt;1) Communication standards - ISO11898-1, ISO11898-2&lt;/P&gt;&lt;P&gt;2) Protocol : CAN2.0B active&lt;/P&gt;&lt;P&gt;3)Format: standard format: ID length 11bit&lt;/P&gt;&lt;P&gt;4)data byte transmission order is big endian&lt;/P&gt;&lt;P&gt;5)Motorola type&lt;/P&gt;&lt;P&gt;6)communication speed:500kbps&lt;/P&gt;&lt;P&gt;7)bit sample point: 72.5 % - 87.5%&lt;/P&gt;&lt;P&gt;8)equipped with high-speed CAN transceiver compliant with ISO11898&lt;/P&gt;&lt;P&gt;9)Terminal resistance:2600ohms.&lt;/P&gt;&lt;P&gt;10)Tolerance shall comply with ISO11898-2&lt;/P&gt;</description>
    <pubDate>Tue, 16 Apr 2024 11:23:58 GMT</pubDate>
    <dc:creator>Nithya_n</dc:creator>
    <dc:date>2024-04-16T11:23:58Z</dc:date>
    <item>
      <title>requesting for isolated CAN controller IC</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/requesting-for-isolated-CAN-controller-IC/m-p/1848073#M22201</link>
      <description>&lt;P&gt;Hi Good Afternoon&lt;BR /&gt;&lt;BR /&gt;Can you suggest the Isolated CAN controller IC's , part number for the below requirements mentioned&lt;/P&gt;&lt;P&gt;1) Communication standards - ISO11898-1, ISO11898-2&lt;/P&gt;&lt;P&gt;2) Protocol : CAN2.0B active&lt;/P&gt;&lt;P&gt;3)Format: standard format: ID length 11bit&lt;/P&gt;&lt;P&gt;4)data byte transmission order is big endian&lt;/P&gt;&lt;P&gt;5)Motorola type&lt;/P&gt;&lt;P&gt;6)communication speed:500kbps&lt;/P&gt;&lt;P&gt;7)bit sample point: 72.5 % - 87.5%&lt;/P&gt;&lt;P&gt;8)equipped with high-speed CAN transceiver compliant with ISO11898&lt;/P&gt;&lt;P&gt;9)Terminal resistance:2600ohms.&lt;/P&gt;&lt;P&gt;10)Tolerance shall comply with ISO11898-2&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 11:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/requesting-for-isolated-CAN-controller-IC/m-p/1848073#M22201</guid>
      <dc:creator>Nithya_n</dc:creator>
      <dc:date>2024-04-16T11:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: requesting for isolated CAN controller IC</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/requesting-for-isolated-CAN-controller-IC/m-p/1848273#M22206</link>
      <description>&lt;P&gt;Hello Nithya,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The only galvanically isolated HS-CAN transceiver in our portfolio is the TJA1052i:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/products/interfaces/can-transceivers/can-with-flexible-data-rate/galvanically-isolated-high-speed-can-transceiver:TJA1052IT" target="_blank" rel="noopener" shape="rect"&gt;https://www.nxp.com/products/interfaces/can-transceivers/can-with-flexible-data-rate/galvanically-isolated-high-speed-can-transceiver:TJA1052IT&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture (3).jpg" style="width: 608px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274093iACE10BECFB2619CE/image-dimensions/608x864?v=v2" width="608" height="864" role="button" title="Capture (3).jpg" alt="Capture (3).jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture (3).jpg&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture 1 (2).jpg" style="width: 587px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274095iBDEDFA794BE7826A/image-dimensions/587x681?v=v2" width="587" height="681" role="button" title="Capture 1 (2).jpg" alt="Capture 1 (2).jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture 1 (2).jpg&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture 2 (1).jpg" style="width: 584px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274096i38302DC0B52BFABB/image-dimensions/584x249?v=v2" width="584" height="249" role="button" title="Capture 2 (1).jpg" alt="Capture 2 (1).jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture 2 (1).jpg&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 15:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/requesting-for-isolated-CAN-controller-IC/m-p/1848273#M22206</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2024-04-16T15:38:31Z</dc:date>
    </item>
  </channel>
</rss>