<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPN532</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN532/m-p/1847270#M22179</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is&amp;nbsp;PN5321A3HN/C106,55 good to go for designing in custom board because previously in the website a few months back&amp;nbsp; I could see&amp;nbsp;PN5321A3HN/C106,55 is NRND?&lt;/P&gt;&lt;P&gt;Also What is the difference between part numbers&amp;nbsp;PN5321A3HN/C106,55 and&amp;nbsp;PN5321A3HN/C106;55 because when I was searching for the stock in octopart I could see the price difference between these two part numberswhere&amp;nbsp;PN5321A3HN/C106,55&amp;nbsp; price is $9.357 and&amp;nbsp;PN5321A3HN/C106;55 price is $8.795?&lt;/P&gt;&lt;P&gt;Also&amp;nbsp; Does&amp;nbsp;PN5321A3HN/C106,55 comes preprogrammed I mean driver code(firmware) loaded into&amp;nbsp;PN5321A3HN/C106,55 so that we can use UART/SPI/I2C protocols to communicate with our custom board MCU or do we need to write entire registers or driver development from scratch?&lt;/P&gt;</description>
    <pubDate>Mon, 15 Apr 2024 15:38:51 GMT</pubDate>
    <dc:creator>Aditya1</dc:creator>
    <dc:date>2024-04-15T15:38:51Z</dc:date>
    <item>
      <title>PN532</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532/m-p/1847270#M22179</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is&amp;nbsp;PN5321A3HN/C106,55 good to go for designing in custom board because previously in the website a few months back&amp;nbsp; I could see&amp;nbsp;PN5321A3HN/C106,55 is NRND?&lt;/P&gt;&lt;P&gt;Also What is the difference between part numbers&amp;nbsp;PN5321A3HN/C106,55 and&amp;nbsp;PN5321A3HN/C106;55 because when I was searching for the stock in octopart I could see the price difference between these two part numberswhere&amp;nbsp;PN5321A3HN/C106,55&amp;nbsp; price is $9.357 and&amp;nbsp;PN5321A3HN/C106;55 price is $8.795?&lt;/P&gt;&lt;P&gt;Also&amp;nbsp; Does&amp;nbsp;PN5321A3HN/C106,55 comes preprogrammed I mean driver code(firmware) loaded into&amp;nbsp;PN5321A3HN/C106,55 so that we can use UART/SPI/I2C protocols to communicate with our custom board MCU or do we need to write entire registers or driver development from scratch?&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 15:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532/m-p/1847270#M22179</guid>
      <dc:creator>Aditya1</dc:creator>
      <dc:date>2024-04-15T15:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: PN532</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN532/m-p/1847357#M22182</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232255"&gt;@Aditya1&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-integrated-solution:PN5321A3HN" target="_blank"&gt;PN5321A3HN&lt;/A&gt; is Not Recommended for New Designs, and the support scope is limited to the information that can be found in the product page. We recommend using &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-plug-and-play-controller-with-integrated-firmware-and-nci-interface:PN7160" target="_blank"&gt;PN7160&lt;/A&gt; instead.&lt;/P&gt;
&lt;P&gt;According to &lt;A href="https://www.nxp.com/part/PN5321A3HN#/" target="_blank"&gt;PN5321A3HN Product Information&lt;/A&gt;, "PN5321A3HN/C106,55" packaging should correspond to &lt;A href="https://www.nxp.com/docs/en/packing/SOT618-1_528.pdf" target="_blank"&gt;TRAY-Tray, Bakeable, Multiple in Drypack&lt;/A&gt;; "PN5321A3HN/C106;55" packaging should correspond to &lt;A href="https://www.nxp.com/docs/en/packing/SOT618-1_551.pdf" target="_blank"&gt;TRAY-Tray, Bakeable, Single in Drypack&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;From &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf" target="_blank"&gt;PN532 Application Note&lt;/A&gt;, Chapter 1 Introduction, this device features a firmware for the different support mode and the required host interfaces (SPI, I2C, HSU).&lt;/P&gt;
&lt;P&gt;If you are still planning to use the device that is Not Recommended for New Designs, please keep in mind that you may face some supply issues in a future.&lt;/P&gt;
&lt;P&gt;I truly apologize for the inconvenience this might cause you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 17:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN532/m-p/1847357#M22182</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-04-15T17:56:16Z</dc:date>
    </item>
  </channel>
</rss>