<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピック56F800 USB TAP error message?</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/56F800-USB-TAP-error-message/m-p/136455#M221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;When trying to program a 56F8322 with the USB tap, I get the following error:&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;Error: Could not write to PRAM, this usually means the wrong configuration file was used&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Well, the correct configuration file is being used, what else could be the cause of this error?&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;This occurs immediately after the "Placing device into debug mode" message, on both the command line "FFLASH.EXE" and with the windows GUI version.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Thanks in advance&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;-Jim&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Nov 2006 07:14:37 GMT</pubDate>
    <dc:creator>JimmyMood</dc:creator>
    <dc:date>2006-11-14T07:14:37Z</dc:date>
    <item>
      <title>56F800 USB TAP error message?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/56F800-USB-TAP-error-message/m-p/136455#M221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;When trying to program a 56F8322 with the USB tap, I get the following error:&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;EM&gt;Error: Could not write to PRAM, this usually means the wrong configuration file was used&lt;/EM&gt;&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Well, the correct configuration file is being used, what else could be the cause of this error?&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;This occurs immediately after the "Placing device into debug mode" message, on both the command line "FFLASH.EXE" and with the windows GUI version.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Thanks in advance&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;-Jim&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Nov 2006 07:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/56F800-USB-TAP-error-message/m-p/136455#M221</guid>
      <dc:creator>JimmyMood</dc:creator>
      <dc:date>2006-11-14T07:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: 56F800 USB TAP error message?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/56F800-USB-TAP-error-message/m-p/136456#M222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;are you using the 56800E Flash programming?&lt;BR /&gt;Are you sure that the config file is the right one (and if it's the right one that is the one coming from the last version of CW)?&lt;BR /&gt;The JTAG clock speed is set right? The flash AFAIK cannot be written if there is a wrong clock speed. I use 800 kHz for parallel port and, I think, 1000 kHz for USBtap (I don't use USBtap so I can't be sure about this).&lt;BR /&gt;&lt;BR /&gt;Let me know&lt;BR /&gt;&lt;BR /&gt;Bye Jack&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2006 18:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/56F800-USB-TAP-error-message/m-p/136456#M222</guid>
      <dc:creator>jag</dc:creator>
      <dc:date>2006-12-20T18:19:01Z</dc:date>
    </item>
  </channel>
</rss>