<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9745B Not High-Impedance When _CS Is High in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-Not-High-Impedance-When-CS-Is-High/m-p/1839346#M21959</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;That's better for analysis if you can show your test schematic here.&lt;/P&gt;</description>
    <pubDate>Tue, 02 Apr 2024 12:22:49 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2024-04-02T12:22:49Z</dc:date>
    <item>
      <title>PCA9745B Not High-Impedance When _CS Is High</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-Not-High-Impedance-When-CS-Is-High/m-p/1837493#M21904</link>
      <description>&lt;P&gt;Similar posts have been made, but not with conclusive responses:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-SDO-high-impedance-state/m-p/994889" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-SDO-high-impedance-state/m-p/994889&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-SDO-stays-low/m-p/1325772" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-SDO-stays-low/m-p/1325772&lt;/A&gt;&lt;/P&gt;&lt;P&gt;We are also observing the&amp;nbsp;PCA9745B SDO pin continue to drive low (not high-impedance, as indicated by the datasheet) when the _CS input is high.&lt;/P&gt;&lt;P&gt;To test this, we isolated the PCA9745B's SDO output (not connected to any other SDO or Master, and connected the pin to a simple voltage divider (10k-ohm to 3.3V and 10k-ohm to GND). In this configuration, we would expect to see ~1.65V if SDO is truly high-impedance.&lt;/P&gt;&lt;P&gt;- After applying power the chip and with _CS HIGH and _RESET HIGH, the SDO pin measures at 0V.&lt;/P&gt;&lt;P&gt;- However, as was mentioned in one of the posts above, if we set _RESET LOW, the SDO pin does measure the expected 1.65V, while the PCA9745B is held in reset. But, as soon as we set _RESET HIGH, the SDO pin drives 0V again.&lt;/P&gt;&lt;P&gt;- Keep in mind, this is the behavior when powering the chip... there is before attempting any SPI communication, so I don't see how there could be a signal-timing issue. When we do attempt SPI communication, the Device properly recieves and processes the data like it should, but when the _CS returns HIGH after communication, the SDO line always drives 0V.&lt;/P&gt;&lt;P&gt;Is this a known issue with this part?&lt;/P&gt;</description>
      <pubDate>Thu, 28 Mar 2024 21:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-Not-High-Impedance-When-CS-Is-High/m-p/1837493#M21904</guid>
      <dc:creator>chrisdums</dc:creator>
      <dc:date>2024-03-28T21:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9745B Not High-Impedance When _CS Is High</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-Not-High-Impedance-When-CS-Is-High/m-p/1839346#M21959</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;That's better for analysis if you can show your test schematic here.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 12:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-Not-High-Impedance-When-CS-Is-High/m-p/1839346#M21959</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-04-02T12:22:49Z</dc:date>
    </item>
  </channel>
</rss>