<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SJA1105 without Host Processor in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105-without-Host-Processor/m-p/1828584#M21638</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;If I understand the datasheet correctly, the&amp;nbsp;&lt;SPAN&gt;SJA1105 Ethernet Switch &lt;EM&gt;requires&amp;nbsp;&lt;/EM&gt;a host processor to load the configuration. This means that I cannot operate the device in a default mode without a processor connected to the SPI port. Did I understand that correctly?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 14 Mar 2024 15:03:23 GMT</pubDate>
    <dc:creator>ttel</dc:creator>
    <dc:date>2024-03-14T15:03:23Z</dc:date>
    <item>
      <title>SJA1105 without Host Processor</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105-without-Host-Processor/m-p/1828584#M21638</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;If I understand the datasheet correctly, the&amp;nbsp;&lt;SPAN&gt;SJA1105 Ethernet Switch &lt;EM&gt;requires&amp;nbsp;&lt;/EM&gt;a host processor to load the configuration. This means that I cannot operate the device in a default mode without a processor connected to the SPI port. Did I understand that correctly?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 15:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105-without-Host-Processor/m-p/1828584#M21638</guid>
      <dc:creator>ttel</dc:creator>
      <dc:date>2024-03-14T15:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105 without Host Processor</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105-without-Host-Processor/m-p/1829139#M21649</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;yes, SJA1105 will not be functional,&amp;nbsp;until the static configuration is successfully loaded via SPI.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 07:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105-without-Host-Processor/m-p/1829139#M21649</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-03-15T07:19:37Z</dc:date>
    </item>
  </channel>
</rss>