<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question about NXP S32v234 plattform in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1818817#M21442</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Correct! there are some issue in synchronization when changes from two cores but, avoid this by change between one core or four core. This correspond to errata ERR050767.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 13:56:35 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-02-29T13:56:35Z</dc:date>
    <item>
      <title>Question about NXP S32v234 plattform</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1817547#M21418</link>
      <description>&lt;P&gt;I'm using nxp s32v234 for multi-core parallel testing but have noticed a performance drop when running dual-core under the same cluster compared to single-core runs, and no drop when running with all cores.&amp;nbsp;The test is each core running a separate application at the same time, The problem is that the performance degradation appears when running dual cores in the same cluster but disappears when running all cores. I'm assuming it could be an issue with the app itself used for testing or a component that plays a role in synchronising when running on multiple cores.&amp;nbsp;Can anyone help me with this?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 14:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1817547#M21418</guid>
      <dc:creator>dortlearner</dc:creator>
      <dc:date>2024-02-28T14:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: Question about NXP S32v234 plattform</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1818817#M21442</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Correct! there are some issue in synchronization when changes from two cores but, avoid this by change between one core or four core. This correspond to errata ERR050767.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 13:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1818817#M21442</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-02-29T13:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Question about NXP S32v234 plattform</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1818836#M21445</link>
      <description>&lt;P&gt;Thanks a lot for your reply. It really helps.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 14:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Question-about-NXP-S32v234-plattform/m-p/1818836#M21445</guid>
      <dc:creator>dortlearner</dc:creator>
      <dc:date>2024-02-29T14:22:56Z</dc:date>
    </item>
  </channel>
</rss>