<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SJA1105TEL MAC Configuration Table (block 09h)、PHY  Address in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1814636#M21330</link>
    <description>&lt;P&gt;PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 23 Feb 2024 12:18:13 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-02-23T12:18:13Z</dc:date>
    <item>
      <title>SJA1105TEL MAC Configuration Table (block 09h)、PHY  Address</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1811762#M21235</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i use SJA1105TEL to design a Ethenter Switch;&lt;/P&gt;&lt;P&gt;1、if i set the&amp;nbsp;MAC Configuration Table (block 09h)&amp;nbsp; all the TOP 、BASE、ENABLE field to&amp;nbsp; 0;&lt;/P&gt;&lt;P&gt;what will happen?&lt;/P&gt;&lt;P&gt;2、if set port0 port1 in phy mode ,how to set the phy address?&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;haiyang&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 08:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1811762#M21235</guid>
      <dc:creator>haiyang</dc:creator>
      <dc:date>2024-02-21T08:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105TEL MAC Configuration Table (block 09h)、PHY  Address</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1812849#M21279</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227461"&gt;@haiyang&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;In case any queue is not enabled for a port, the forwarded frame which is assigned to this queue is dropped. &lt;BR /&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 13:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1812849#M21279</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-21T13:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105TEL MAC Configuration Table (block 09h)、PHY  Address</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1812860#M21280</link>
      <description>&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;thanks reply ，i see your point！&lt;/P&gt;&lt;P&gt;and the second question ，how to set&amp;nbsp;&lt;/P&gt;&lt;P&gt;the phy address for port0 and port1, when they set to phy mode？&lt;/P&gt;&lt;P&gt;in my memory，the SJA1105P &amp;nbsp;can set address through some config pin，but the&amp;nbsp;&lt;/P&gt;&lt;P&gt;SJA1105TEL have no these pin&lt;/P&gt;&lt;P&gt;best wish&lt;/P&gt;&lt;P&gt;haiyang&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 14:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1812860#M21280</guid>
      <dc:creator>haiyang</dc:creator>
      <dc:date>2024-02-21T14:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105TEL MAC Configuration Table (block 09h)、PHY  Address</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1814636#M21330</link>
      <description>&lt;P&gt;PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 23 Feb 2024 12:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1105TEL-MAC-Configuration-Table-block-09h-PHY-Address/m-p/1814636#M21330</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-23T12:18:13Z</dc:date>
    </item>
  </channel>
</rss>