<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 192kHz sampling rate on the Soundbite board in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204366#M2133</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that AK4584 does not support 192K ADC but it do can generate&lt;BR /&gt;LRCLK/BCLK clock for AK4556.&lt;BR /&gt;&lt;BR /&gt;From the features list of AK4584 data sheet(&lt;BR /&gt;&lt;A href="http://datasheet.digchip.com/025/025-00607-0-AK4584.pdf)" target="test_blank"&gt;http://datasheet.digchip.com/025/025-00607-0-AK4584.pdf)&lt;/A&gt; we can see that&lt;BR /&gt;this codec&lt;BR /&gt;1. Support 24bit 2ch&amp;nbsp; 96K ADC, 192K DIR&lt;BR /&gt;2. Support 24bit 2ch 192K DAC, 192K DIT&lt;BR /&gt;&lt;BR /&gt;In order to support 192K, we should use 128fs mode and quad speed&amp;nbsp; mode as&lt;BR /&gt;well. In the section "System clock", that mentioned "The ADC is&lt;BR /&gt;powered down&lt;BR /&gt;during quad speed mode".&lt;BR /&gt;&lt;BR /&gt;AK4556 clock has been configured as slave move with CKS3:0 = 0100. It should&lt;BR /&gt;support fs=192K.&lt;/P&gt;&lt;DIV&gt;I&amp;nbsp;also have tried that on my two Soundbite boards.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;One is ok to generate&amp;nbsp;192k clock and get proper output&amp;nbsp;for I/Os 3 to 8 with I/Os 1 and 2 'muted'.&lt;/DIV&gt;&lt;DIV&gt;Another one only generate 44.1K clock. I think the&amp;nbsp;second board must&amp;nbsp;have something wrong with codec. I didn't do further test on that. Perhaps we can read back all register setting from codec to double check it.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Aug 2009 22:07:07 GMT</pubDate>
    <dc:creator>JohnnyChen</dc:creator>
    <dc:date>2009-08-07T22:07:07Z</dc:date>
    <item>
      <title>192kHz sampling rate on the Soundbite board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204365#M2132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, I need to enable analog inputs with 192kHz sampling rate on the Soundbite board. I use the the standard Freescale template application configures AK4584 to generate the sampling clock for all components. In the template code I have found options for 96, 64, 48 kHz only. In my understanding I need to reconfigure the Clock Mode Control register on AK4584. Could somenody advise the proper setting for 192 kHz?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2009 07:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204365#M2132</guid>
      <dc:creator>petr_sh</dc:creator>
      <dc:date>2009-08-01T07:33:25Z</dc:date>
    </item>
    <item>
      <title>Re: 192kHz sampling rate on the Soundbite board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204366#M2133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please note that AK4584 does not support 192K ADC but it do can generate&lt;BR /&gt;LRCLK/BCLK clock for AK4556.&lt;BR /&gt;&lt;BR /&gt;From the features list of AK4584 data sheet(&lt;BR /&gt;&lt;A href="http://datasheet.digchip.com/025/025-00607-0-AK4584.pdf)" target="test_blank"&gt;http://datasheet.digchip.com/025/025-00607-0-AK4584.pdf)&lt;/A&gt; we can see that&lt;BR /&gt;this codec&lt;BR /&gt;1. Support 24bit 2ch&amp;nbsp; 96K ADC, 192K DIR&lt;BR /&gt;2. Support 24bit 2ch 192K DAC, 192K DIT&lt;BR /&gt;&lt;BR /&gt;In order to support 192K, we should use 128fs mode and quad speed&amp;nbsp; mode as&lt;BR /&gt;well. In the section "System clock", that mentioned "The ADC is&lt;BR /&gt;powered down&lt;BR /&gt;during quad speed mode".&lt;BR /&gt;&lt;BR /&gt;AK4556 clock has been configured as slave move with CKS3:0 = 0100. It should&lt;BR /&gt;support fs=192K.&lt;/P&gt;&lt;DIV&gt;I&amp;nbsp;also have tried that on my two Soundbite boards.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;One is ok to generate&amp;nbsp;192k clock and get proper output&amp;nbsp;for I/Os 3 to 8 with I/Os 1 and 2 'muted'.&lt;/DIV&gt;&lt;DIV&gt;Another one only generate 44.1K clock. I think the&amp;nbsp;second board must&amp;nbsp;have something wrong with codec. I didn't do further test on that. Perhaps we can read back all register setting from codec to double check it.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2009 22:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204366#M2133</guid>
      <dc:creator>JohnnyChen</dc:creator>
      <dc:date>2009-08-07T22:07:07Z</dc:date>
    </item>
    <item>
      <title>Re: 192kHz sampling rate on the Soundbite board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204367#M2134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The configuration settings&amp;nbsp;Freescale Support team&amp;nbsp;provided for AK4584 correctly&amp;nbsp; generate clocks for AK4556 (the changed part in the configuration is: REG#&amp;gt;9=$A6; REG#&amp;gt;2=$E). I can see LRCLK is 192KHz. I use the audio processing chain: J3-&amp;gt;U2(AK4556)-&amp;gt;U1(DSP56371)-&amp;gt;U2-&amp;gt;J4. And the assembly template application works well with them, it passes through the 1KHz sine wave pretty clearly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, the problem is with the C-template application. It corrupts the input sine wave (applied to J3 input for the instance) even sampling at 96KHz, and in the more severe way at 192KHZ. So, I think there is a problem in the Soundbite C-template application in the way it configures the HW or processes the interrupts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Aug 2009 04:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/192kHz-sampling-rate-on-the-Soundbite-board/m-p/204367#M2134</guid>
      <dc:creator>petr_sh</dc:creator>
      <dc:date>2009-08-09T04:58:07Z</dc:date>
    </item>
  </channel>
</rss>