<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic STM32U585 VDDIO2 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/STM32U585-VDDIO2/m-p/1812085#M21239</link>
    <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I am using the STM32U585 in a design, and I have VDD at 3.3V and VDDIO2 at 1.8V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The 1.8V rail is supplied by a 3.3V to 1.8V voltage regulator. I connected the Enable of this voltage regulator to one of the STM32U585 I/O (this I/O isn't on the PG port, because PG port is supplied by VDDIO2). Do you foresee any problem with this setup? I mean the 3.3V will turn on at first, and then the STM32 will turn on the 1.8V regulator, which supply VDDIO2 rail.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;In the datasheet it is clear that, VDDIO2 and VDD are two independent supplies. I just want a confirmation, and if someone here has a similar implementation in a working design.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ballimo&lt;/P&gt;</description>
    <pubDate>Tue, 20 Feb 2024 17:04:53 GMT</pubDate>
    <dc:creator>Ballimo</dc:creator>
    <dc:date>2024-02-20T17:04:53Z</dc:date>
    <item>
      <title>STM32U585 VDDIO2</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/STM32U585-VDDIO2/m-p/1812085#M21239</link>
      <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;I am using the STM32U585 in a design, and I have VDD at 3.3V and VDDIO2 at 1.8V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The 1.8V rail is supplied by a 3.3V to 1.8V voltage regulator. I connected the Enable of this voltage regulator to one of the STM32U585 I/O (this I/O isn't on the PG port, because PG port is supplied by VDDIO2). Do you foresee any problem with this setup? I mean the 3.3V will turn on at first, and then the STM32 will turn on the 1.8V regulator, which supply VDDIO2 rail.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;In the datasheet it is clear that, VDDIO2 and VDD are two independent supplies. I just want a confirmation, and if someone here has a similar implementation in a working design.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ballimo&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 17:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/STM32U585-VDDIO2/m-p/1812085#M21239</guid>
      <dc:creator>Ballimo</dc:creator>
      <dc:date>2024-02-20T17:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: STM32U585 VDDIO2</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/STM32U585-VDDIO2/m-p/1812141#M21245</link>
      <description>&lt;P&gt;STM32U585 does not belong to the NXP portfolio and belongs to STMicroelectronics, please contact them for further support.&lt;/P&gt;&lt;P&gt;I'm sorry for the inconvenience this may cause&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Tech support&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 18:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/STM32U585-VDDIO2/m-p/1812141#M21245</guid>
      <dc:creator>Alondra</dc:creator>
      <dc:date>2024-02-20T18:47:02Z</dc:date>
    </item>
  </channel>
</rss>