<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: libusb error while flashing iMX6ULL NAND device using UUU</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1805033#M21088</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;;&lt;/P&gt;&lt;P&gt;I tried what you suggested, but still I am facing the similar issue.&lt;/P&gt;&lt;P&gt;Can you suggest whether the issue is with the u-boot which I am building or something related to usb driver on host?&lt;/P&gt;&lt;P&gt;Attaching the generated u-boot for your reference.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;-Ali&lt;/P&gt;</description>
    <pubDate>Sun, 11 Feb 2024 09:02:48 GMT</pubDate>
    <dc:creator>asurti9</dc:creator>
    <dc:date>2024-02-11T09:02:48Z</dc:date>
    <item>
      <title>libusb error while flashing iMX6ULL NAND device using UUU</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1801215#M21001</link>
      <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;I am trying to flash my custom &lt;LI-PRODUCT title="iMX6ULL" id="iMX6ULL"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;devicehaving NAND flash. It is based on iMX6ULL EVK design&lt;/P&gt;&lt;P&gt;I have downloaded the YOCTO source and built it with UBOOT_CONFIG = "nand" in local.conf.&lt;/P&gt;&lt;P&gt;The image generated is&amp;nbsp;u-boot-nand-2023.04-r0.imx&lt;/P&gt;&lt;P&gt;When I try flashing the device with the above mentioned u-boot, I am facing below error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sudo uuu -v -V -pp 1 -b nand u-boot-nand-2023.04-r0.imx
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Build in config:
	Pctl	 Chip		 Vid	 Pid	 BcdVersion
	==================================================
	SDPS:	 MX8QXP		 0x1fc9	 0x012f	 [0x0002..0xffff]
	SDPS:	 MX8QM		 0x1fc9	 0x0129	 [0x0002..0xffff]
	SDPS:	 MX8DXL		 0x1fc9	 0x0147
	SDPS:	 MX28		 0x15a2	 0x004f
	SDPS:	 MX815		 0x1fc9	 0x013e
	SDPS:	 MX865		 0x1fc9	 0x0146
	SDPS:	 MX8ULP		 0x1fc9	 0x014a
	SDPS:	 MX8ULP		 0x1fc9	 0x014b
	SDPS:	 MX93		 0x1fc9	 0x014e
	SDP:	 MX7D		 0x15a2	 0x0076
	SDP:	 MX6Q		 0x15a2	 0x0054
	SDP:	 MX6D		 0x15a2	 0x0061
	SDP:	 MX6SL		 0x15a2	 0x0063
	SDP:	 MX6SX		 0x15a2	 0x0071
	SDP:	 MX6UL		 0x15a2	 0x007d
	SDP:	 MX6ULL		 0x15a2	 0x0080
	SDP:	 MX6SLL		 0x1fc9	 0x0128
	SDP:	 MX7ULP		 0x1fc9	 0x0126
	SDP:	 MXRT106X	 0x1fc9	 0x0135
	SDP:	 MX8MM		 0x1fc9	 0x0134
	SDP:	 MX8MQ		 0x1fc9	 0x012b
	SDPU:	 SPL		 0x0525	 0xb4a4	 [0x0000..0x04ff]
	SDPV:	 SPL1		 0x0525	 0xb4a4	 [0x0500..0x9998]
	SDPV:	 SPL1		 0x1fc9	 0x0151	 [0x0500..0x9998]
	SDPU:	 SPL		 0x0525	 0xb4a4	 [0x9999..0x9999]
	SDPU:	 SPL		 0x3016	 0x1001	 [0x0000..0x04ff]
	SDPV:	 SPL1		 0x3016	 0x1001	 [0x0500..0x9998]
	FBK:	 		 0x066f	 0x9afe
	FBK:	 		 0x066f	 0x9bff
	FBK:	 		 0x1fc9	 0x0153
	FB:	 		 0x0525	 0xa4a5
	FB:	 		 0x18d1	 0x0d02
	FB:	 		 0x3016	 0x0001
	FB:	 		 0x1fc9	 0x0152
	FB:	 		 0x0483	 0x0afb

Run built-in script:
 
uuu_version 1.2.39

# @_flash.bin            | bootloader
# @_image   [_flash.bin] | image burn to nand, default is the same as bootloader

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f u-boot-nand-2023.04-r0.imx

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f u-boot-nand-2023.04-r0.imx

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f u-boot-nand-2023.04-r0.imx -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f u-boot-nand-2023.04-r0.imx -skipspl
SDPV: jump
# }

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f u-boot-nand-2023.04-r0.imx
FB: ucmd if test ! -n "$fastboot_bytes"; then setenv fastboot_bytes $filesize; else true; fi
# Burn image to nandfit partition if needed
FB: ucmd if env exists nandfit_part; then nand erase.part nandfit; nand write ${fastboot_buffer} nandfit ${fastboot_bytes}; else true; fi;
FB: ucmd nandbcb init ${fastboot_buffer} nandboot ${fastboot_bytes}
FB: Done


Wait for Known USB Device Appear...
New USB Device Attached at 1:13
1:13&amp;gt;Start Cmd:SDP: boot -f u-boot-nand-2023.04-r0.imx
100%1:13&amp;gt;Okay (0.318s)
New USB Device Attached at 1:13
1:13&amp;gt;Start Cmd:SDP: boot -f u-boot-nand-2023.04-r0.imx
100%libusb: error [udev_hotplug_event] ignoring udev action bind
1:13&amp;gt;Fail HID(R):LIBUSB_ERROR_TIMEOUT(1.003s)&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried the prebuilt images from &lt;A href="https://www.nxp.com/webapp/Download?colCode=L6.1.55_2.2.0_MX6UL7D&amp;amp;appType=license&amp;amp;_gl=1*1gzao0p*_ga*ODM2MDcyNjUxLjE3MDY5NjA4OTQ.*_ga_WM5LE0KMSH*MTcwNjk2MDg5NC4xLjEuMTcwNjk2MTE2OC4wLjAuMA.." target="_self"&gt;NXP&lt;/A&gt;&amp;nbsp;, but it is also giving the same error. I tried the example uuu script as well, with the modifications needed. But I am facing the same issue.&lt;/P&gt;&lt;P&gt;If needed I can share the schematic of our custom board privately to get it reviewed.&lt;/P&gt;&lt;P&gt;Can you please help us resolving the issue?&lt;/P&gt;&lt;P&gt;Thanks!&lt;BR /&gt;- Ali&lt;/P&gt;</description>
      <pubDate>Sat, 03 Feb 2024 12:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1801215#M21001</guid>
      <dc:creator>asurti9</dc:creator>
      <dc:date>2024-02-03T12:00:51Z</dc:date>
    </item>
    <item>
      <title>Re: libusb error while flashing iMX6ULL NAND device using UUU</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1802191#M21024</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You could try &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-To-use-NAND-boot-on-i-MX6UL-EVK-board/ta-p/1116178" target="_self"&gt;this porting guide&lt;/A&gt; but for 6ULL, i.e., you have to make modifications to support 6ULL's nand boot and there are in latest release as:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/7376547b9e424b2d0f42dfe96394168c781ca297/configs/mx6ull_14x14_evk_nand_defconfig#L10" target="_self"&gt;configs/mx6ull_14x14_evk_nand_defconfig&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In that case, you'd take upon the test and update to latest release and latest UUU release, please update how did it went.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 00:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1802191#M21024</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-02-06T00:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: libusb error while flashing iMX6ULL NAND device using UUU</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1805033#M21088</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;;&lt;/P&gt;&lt;P&gt;I tried what you suggested, but still I am facing the similar issue.&lt;/P&gt;&lt;P&gt;Can you suggest whether the issue is with the u-boot which I am building or something related to usb driver on host?&lt;/P&gt;&lt;P&gt;Attaching the generated u-boot for your reference.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;-Ali&lt;/P&gt;</description>
      <pubDate>Sun, 11 Feb 2024 09:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/libusb-error-while-flashing-iMX6ULL-NAND-device-using-UUU/m-p/1805033#M21088</guid>
      <dc:creator>asurti9</dc:creator>
      <dc:date>2024-02-11T09:02:48Z</dc:date>
    </item>
  </channel>
</rss>