<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックReactivation of DMA Tx and Rx channel when configured with SPI on IMXRT1060</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Reactivation-of-DMA-Tx-and-Rx-channel-when-configured-with-SPI/m-p/1784576#M20728</link>
    <description>&lt;P&gt;I configured DMA with SPI master to transfer and receive data on LPSPI4. I have transmitted data from a hard coded array data&amp;nbsp; and it is transmitted successfully and data also received from MISO.&lt;/P&gt;&lt;P&gt;My final goal is to transmit same array in an infinite manner i.e I want to reactivate TX channel to send the array elements again ans reactivate RX channel to receive MISO data.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried channel linking to reactivate same channel again but its not working for me.&lt;/P&gt;&lt;P&gt;I tried Trigger mode of DMa also but it was also not working.&lt;/P&gt;&lt;P&gt;If any example or document can shared it would be good.&lt;/P&gt;&lt;P&gt;Also wanted to know that Is there any cpu overhead if we use trigger mode instead of channel linking for my scenario?&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jan 2024 17:41:39 GMT</pubDate>
    <dc:creator>jkaur38</dc:creator>
    <dc:date>2024-01-08T17:41:39Z</dc:date>
    <item>
      <title>Reactivation of DMA Tx and Rx channel when configured with SPI on IMXRT1060</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Reactivation-of-DMA-Tx-and-Rx-channel-when-configured-with-SPI/m-p/1784576#M20728</link>
      <description>&lt;P&gt;I configured DMA with SPI master to transfer and receive data on LPSPI4. I have transmitted data from a hard coded array data&amp;nbsp; and it is transmitted successfully and data also received from MISO.&lt;/P&gt;&lt;P&gt;My final goal is to transmit same array in an infinite manner i.e I want to reactivate TX channel to send the array elements again ans reactivate RX channel to receive MISO data.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried channel linking to reactivate same channel again but its not working for me.&lt;/P&gt;&lt;P&gt;I tried Trigger mode of DMa also but it was also not working.&lt;/P&gt;&lt;P&gt;If any example or document can shared it would be good.&lt;/P&gt;&lt;P&gt;Also wanted to know that Is there any cpu overhead if we use trigger mode instead of channel linking for my scenario?&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jan 2024 17:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Reactivation-of-DMA-Tx-and-Rx-channel-when-configured-with-SPI/m-p/1784576#M20728</guid>
      <dc:creator>jkaur38</dc:creator>
      <dc:date>2024-01-08T17:41:39Z</dc:date>
    </item>
    <item>
      <title>回复： Reactivation of DMA Tx and Rx channel when configured with SPI on IMXRT1060</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Reactivation-of-DMA-Tx-and-Rx-channel-when-configured-with-SPI/m-p/1786952#M20768</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227796"&gt;@jkaur38&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series.&lt;/P&gt;
&lt;P&gt;For the second question, using the trigger method does consume some CPU, the channel link method does not, so the channel link method is recommended.&lt;/P&gt;
&lt;P&gt;For the first question, can you post the main modification code for the channel connection method?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 07:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Reactivation-of-DMA-Tx-and-Rx-channel-when-configured-with-SPI/m-p/1786952#M20768</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-01-11T07:41:09Z</dc:date>
    </item>
  </channel>
</rss>