<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: mmc initialization error with SD Card on LS1046ARDB based board</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1768877#M20352</link>
    <description>&lt;P&gt;Do you use LSDK 21.08 pre-build image downloaded from the following link?&lt;/P&gt;
&lt;P&gt;wget &lt;A href="https://www.nxp.com/lgfiles/sdk/lsdk2108/lsdk2108_yocto_tiny_LS_arm64.itb" target="_blank"&gt;https://www.nxp.com/lgfiles/sdk/lsdk2108/lsdk2108_yocto_tiny_LS_arm64.itb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I verified this image on LS1046ARDB, there is no problem, please refer to the attachment.&lt;/P&gt;
&lt;P&gt;Please try LSDK 21.08 u-boot(ATF) image and check whether this problem persists.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 08:52:05 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-12-05T08:52:05Z</dc:date>
    <item>
      <title>mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1765643#M20291</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;Iam using a custom board based on LS1046ARDB, we have copied the schematics of LS1046ARDB for SD Card Section,&lt;/P&gt;&lt;P&gt;I have copied the firmware image in to the QSPI, and i have set the mmc storage as sd card.&lt;/P&gt;&lt;P&gt;In uboot the SD card is detecting perfectly, following are the u-boot status&lt;/P&gt;&lt;P&gt;=&amp;gt; mmcinfo&lt;BR /&gt;Device: FSL_SDHC&lt;BR /&gt;Manufacturer ID: 3&lt;BR /&gt;OEM: 5344&lt;BR /&gt;Name: SC16G&lt;BR /&gt;Bus Speed: 50000000&lt;BR /&gt;Mode: SD High Speed (50MHz)&lt;BR /&gt;Rd Block Len: 512&lt;BR /&gt;SD version 3.0&lt;BR /&gt;High Capacity: Yes&lt;BR /&gt;Capacity: 14.8 GiB&lt;BR /&gt;Bus Width: 4-bit&lt;BR /&gt;Erase Group Size: 512 Bytes&lt;/P&gt;&lt;P&gt;However, when i boot further the OS boots, but the SD card is not getting detected, when i do dmesg for mmc below message is displayed (&lt;STRONG&gt;Complete boot log to Tiny Linux for 16GB SD Card is attached&lt;/STRONG&gt;)&lt;/P&gt;&lt;P&gt;root@TinyLinux:~# dmesg | grep mmc&lt;BR /&gt;[ 3.443041] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit&lt;BR /&gt;[ 3.533641] mmc0: error -110 whilst initialising SD card&lt;/P&gt;&lt;P&gt;Also please note that in the same SD card , if iam installing Bootpartition and rootfs files and then booting, then the OS boots perfectly and SD card is also detected (&lt;STRONG&gt;attached is the log of the linux OS&lt;/STRONG&gt; for the same SD card).&lt;/P&gt;&lt;P&gt;From above it is clear that the there is no problem in the SD Card nor the hardware, i feel there is some configurations in the firmware image which iam missing, please let me know what can be done to remove this initialising SD card error, in Tiny Linux.&lt;/P&gt;&lt;P&gt;Please provide your help/support&lt;/P&gt;&lt;P&gt;Thank u.&lt;/P&gt;</description>
      <pubDate>Wed, 29 Nov 2023 11:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1765643#M20291</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2023-11-29T11:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1767881#M20329</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;Awaiting for your help/support,&lt;/P&gt;&lt;P&gt;Please provide your help.&lt;/P&gt;&lt;P&gt;Thank u&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 05:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1767881#M20329</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2023-12-04T05:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1768877#M20352</link>
      <description>&lt;P&gt;Do you use LSDK 21.08 pre-build image downloaded from the following link?&lt;/P&gt;
&lt;P&gt;wget &lt;A href="https://www.nxp.com/lgfiles/sdk/lsdk2108/lsdk2108_yocto_tiny_LS_arm64.itb" target="_blank"&gt;https://www.nxp.com/lgfiles/sdk/lsdk2108/lsdk2108_yocto_tiny_LS_arm64.itb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I verified this image on LS1046ARDB, there is no problem, please refer to the attachment.&lt;/P&gt;
&lt;P&gt;Please try LSDK 21.08 u-boot(ATF) image and check whether this problem persists.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 08:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1768877#M20352</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-12-05T08:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1768991#M20356</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;thank u for the reply,&lt;/P&gt;&lt;P&gt;I have used the itb from the link provided and build the firmware image freshly(refer below commands), but the issue still persists (refer attached boot log), please let me know what can be done.&lt;/P&gt;&lt;P&gt;MACHINE: ls1046ardb&lt;BR /&gt;BOOTTYPE: sd&lt;BR /&gt;Writing 0x00000000 &amp;lt;---&amp;gt; firmware/atf/ls1046ardb/bl2_sd.pbl&lt;BR /&gt;Writing 0x00100000 &amp;lt;---&amp;gt; firmware/atf/ls1046ardb/fip_uboot.bin&lt;BR /&gt;Writing 0x00900000 &amp;lt;---&amp;gt; firmware/fm_ucode/fsl_fman_ucode_ls1046_r1.0_106_4_18.bin&lt;BR /&gt;Writing 0x00940000 &amp;lt;---&amp;gt; firmware/qe_ucode/iram_Type_A_LS1021a_r1.0.bin&lt;BR /&gt;Writing 0x00980000 &amp;lt;---&amp;gt; firmware/phy_cortina/cs4315-cs4340-PHY-ucode.txt&lt;BR /&gt;Writing 0x009C0000 &amp;lt;---&amp;gt; images/flash_images.scr&lt;BR /&gt;Writing 0x00F00000 &amp;lt;---&amp;gt; linux/kernel/arm64/LS/fsl-ls1046a-rdb-sdk.dtb&lt;BR /&gt;Writing 0x01000000 &amp;lt;---&amp;gt; images/lsdk2108_yocto_tiny_LS_arm64.itb&lt;BR /&gt;/home/ghouse/flexbuild_lsdk2108/build/images/firmware_ls1046ardb_sdboot.img [Done]&lt;/P&gt;&lt;P&gt;Thank u.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 11:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1768991#M20356</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2023-12-05T11:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1771513#M20419</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Any update on this? please provide your help/support.&lt;/P&gt;&lt;P&gt;Thank u&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 10:56:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1771513#M20419</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2023-12-08T10:56:44Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1771530#M20420</link>
      <description>&lt;P&gt;I checked your previous logs, you are using different Kernel image in these two files.&lt;/P&gt;&lt;P&gt;[ 0.000000] Linux version 5.10.35-dirty (ghouse@ghouse-pc) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.2) 9.4.03&lt;/P&gt;&lt;P&gt;Linux version 5.10.35 (ghouse@ghouse-pc) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.1) 9.4.0, GNU 2&lt;/P&gt;&lt;P&gt;Please use Kernel images and dts files provided in&amp;nbsp;log_16gbsd_linux.log to generate itb file.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Dec 2023 12:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1771530#M20420</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-12-08T12:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: mmc initialization error with SD Card on LS1046ARDB based board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1772143#M20431</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the reply,&lt;/P&gt;&lt;P&gt;I deleted the existing itd file and recompiled the Firmware Image, now iam able to detect the SD card in Tiny linux also.&lt;/P&gt;&lt;P&gt;Thank u very much for the support extended by you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank u.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 09:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mmc-initialization-error-with-SD-Card-on-LS1046ARDB-based-board/m-p/1772143#M20431</guid>
      <dc:creator>Ghouse</dc:creator>
      <dc:date>2023-12-11T09:17:41Z</dc:date>
    </item>
  </channel>
</rss>