<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ptn5150A usb 3.2 connection fail in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1767983#M20333</link>
    <description>&lt;P&gt;Hello Jozef,&lt;/P&gt;&lt;P&gt;i connected pin 4 to VBUS of the connector and steel it don't work.&lt;/P&gt;&lt;P&gt;i let the pin 4 floating and now i recognized the camera in DFP mode but i don't think that it's ok.&lt;/P&gt;&lt;P&gt;if you can , i need application note of DFP mode how to connect pin 4 because now is floating and it's work and when i connect him to VBUS of USB it don't work but i don't think it's ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;</description>
    <pubDate>Mon, 04 Dec 2023 06:55:08 GMT</pubDate>
    <dc:creator>gady</dc:creator>
    <dc:date>2023-12-04T06:55:08Z</dc:date>
    <item>
      <title>ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761740#M20203</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i have 2 cards , one of them is Host who is connected to PC and the second is Device&amp;nbsp;that connect a camera to it. i use on both modules the chip PTN5150A to connect between them via a cable of HDBAST , and cables type C.&lt;/P&gt;&lt;P&gt;the problem is that the chip on Device is not working , it don't recognize the Host so i don't have connection of the camera to pc.&lt;/P&gt;&lt;P&gt;i attach her the block diagram and the schematic.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 08:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761740#M20203</guid>
      <dc:creator>gady</dc:creator>
      <dc:date>2023-11-22T08:45:01Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761925#M20206</link>
      <description>&lt;P&gt;Hello Gad,&lt;/P&gt;
&lt;P&gt;I suppose you want to use a non-I2C mode. In this case, the ADR pin must be floating during power up. Please refer to the section 7.5 in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/PTN5150A.pdf" target="_self"&gt;PTN5150A datasheet&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please consider purchasing &lt;A href="http://OM13584" target="_self"&gt;OM13584&lt;/A&gt; for evaluation. You can take the OM13584 schematic as a reference.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 12:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761925#M20206</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-11-22T12:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761952#M20207</link>
      <description>&lt;P&gt;Hello Jozef,&lt;/P&gt;&lt;P&gt;according the datasheet of PTN5150A the pn ADR must be floating or mid so i can use him to be output and get indication if there is connection.&lt;/P&gt;&lt;P&gt;about the OM13584 i see the schematic as a reference but it's for type-c to type-a, in this case it's work. my problem is the connection of type-c to type-c (host and device has type-c connector and the same chip). pin PORT in host is connected to PULL-DOWN (UFP) and the device the pin PORT is connected to PULL-UP (DFP) and i don't have a connection between him/&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 13:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1761952#M20207</guid>
      <dc:creator>gady</dc:creator>
      <dc:date>2023-11-22T13:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1763730#M20244</link>
      <description>&lt;P&gt;Hello Gady,&lt;/P&gt;
&lt;P&gt;please see below an answer from an application engineer I have contacted.&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;The problem is that the chip on Device is not working , it don't recognize the Host so I don't have connection of the camera to pc.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;[A] Customer will need to change the device board’s PTN5150 PORT pin to pull high (to make if DFP, so it can detect a device plug into the port) – if not possible to change to pull up, then at least leave it as floating (remove the pull down resistor R61 ) , then PTN5150 will work as DRP mode, and still able to detect the camera.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;According the datasheet of PTN5150A the pin ADR must be floating or mid so I can use him to be output and get indication if there is connection.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;[A] THAT’S correct.&amp;nbsp; Since I don’t see customer use I2C, then they should not pull up or pull down the ADR pin.&amp;nbsp; (and by the way, you can’t pull up R57 to VBUS level.&amp;nbsp; It is not correct)&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1701062489134.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251525iDF7E21E13BC8C611/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1701062489134.png" alt="JozefKozon_0-1701062489134.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;About the OM13584 I see the schematic as a reference but it's for type-c to type-a, in this case it's work. my problem is the connection of type-c to type-c (host and device has type-c connector and the same chip). pin PORT in host is connected to PULL-DOWN (UFP) and the device the pin PORT is connected to PULL-UP (DFP) and I don't have a connection between him/&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;[A] I don’t understand this part of the problem.&amp;nbsp; “pin PORT in host is connected to PULL-DOWN (UFP) and the device the pin PORT is connected to PULL-UP (DFP)” -&amp;gt; this is correct.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;-&amp;gt; “I don't have a connection between him/”&amp;nbsp; -&amp;gt; not sure what this means here.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 05:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1763730#M20244</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-11-27T05:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1764650#M20274</link>
      <description>&lt;P&gt;Hello Jozef,&lt;/P&gt;&lt;P&gt;thank you for the help you give.&lt;/P&gt;&lt;P&gt;i have only one issue : the PTN5150A don't recognized connection with camera in mode DFP or DRP&lt;/P&gt;&lt;P&gt;- pin 3 (port) and pin 5 (ADR) are floating&lt;/P&gt;&lt;P&gt;- pin 4 (Vbus_det) are connected to resistor 1M to VDD&amp;nbsp;&lt;/P&gt;&lt;P&gt;sop i don't have connection with USB3.2&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 07:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1764650#M20274</guid>
      <dc:creator>gady</dc:creator>
      <dc:date>2023-11-28T07:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1766942#M20319</link>
      <description>&lt;P&gt;Hello Gady,&lt;/P&gt;
&lt;P&gt;I have sent your reply to the application engineer. As soon as he answers me, I will definitely reply to you.&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 05:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1766942#M20319</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-12-01T05:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1767898#M20332</link>
      <description>&lt;P&gt;Hello Gady,&lt;/P&gt;
&lt;P&gt;please see below an answer from the application engineer.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;- pin 3 (port) and pin 5 (ADR) are floating&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;[A] This is fine&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;- pin 4 (Vbus_det) are connected to resistor &lt;STRONG&gt;1M to VDD&lt;/STRONG&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;[A] this might not be a good idea. My question is, for the device, the board needs to provide VBUS power to the device.&amp;nbsp; How is this done?&amp;nbsp; Is there a source FET here to output 5V VBUS to the device side’s Type-C.&amp;nbsp; I don’t see that part of the schematics.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;Even we are using PTN5150 in DRP mode, the state machine still look at the VBUS voltage.&amp;nbsp; So pin 4 should connect to a resistor 1M to VBUS.&amp;nbsp; You can’t tie it to VDD all the time.&amp;nbsp; (VBUS is only turned on when there is connection, and VBUS should be off when there is no connection.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 05:45:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1767898#M20332</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-12-04T05:45:52Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1767983#M20333</link>
      <description>&lt;P&gt;Hello Jozef,&lt;/P&gt;&lt;P&gt;i connected pin 4 to VBUS of the connector and steel it don't work.&lt;/P&gt;&lt;P&gt;i let the pin 4 floating and now i recognized the camera in DFP mode but i don't think that it's ok.&lt;/P&gt;&lt;P&gt;if you can , i need application note of DFP mode how to connect pin 4 because now is floating and it's work and when i connect him to VBUS of USB it don't work but i don't think it's ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 06:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1767983#M20333</guid>
      <dc:creator>gady</dc:creator>
      <dc:date>2023-12-04T06:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: ptn5150A usb 3.2 connection fail</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1768725#M20348</link>
      <description>&lt;P&gt;Hello Gady,&lt;/P&gt;
&lt;P&gt;please see an answer from the application engineer.&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;You need a load switch to turn on turn off the VBUS, in reference to the schematics attached, ou will need to have&lt;/FONT&gt;&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;&lt;FONT color="#0000FF"&gt;U2 – load switch to turn on/off the VBUS based on time of connection&lt;/FONT&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;FONT color="#0000FF"&gt;U3 – logic to enable/disable the load switch (currently, logic is based on CON_DET &amp;amp;&amp;amp; /USB2_ID&lt;/FONT&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;Hope this helps.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 05:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ptn5150A-usb-3-2-connection-fail/m-p/1768725#M20348</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-12-05T05:34:01Z</dc:date>
    </item>
  </channel>
</rss>