<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FS2633 WAKE UP in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/FS2633-WAKE-UP/m-p/1758697#M20135</link>
    <description>&lt;P&gt;Hello Team, I am using FS2633, there are three questions about FS26 LPOFF mode wake-up :&lt;BR /&gt;FS26 LPOFF mode wake-up issue, 0x57 register read value=0x2009:&lt;BR /&gt;1: Power on to call Sbc_ Fs26_ The SetOperatingMode function allows you to enter LPOFF mode normally.&lt;BR /&gt;2: After powering on and operating other registers, call Sbc again_ Fs26_ The SetOperatingMode function is invalid when it enters LPOFF. (CRC verification is normal, and the oscilloscope has checked that there is no fluctuation in the output voltage.)&lt;BR /&gt;3: In debug mode, clearing the wake-up source and configuring the wake-up source ensures that the wake-up source is currently at a low level,&lt;BR /&gt;Call Sbc again_ Fs26_ SetOperatingMode failed to enter LPOFF mode, and the output voltage was checked through an oscilloscope without any fluctuations.&lt;/P&gt;</description>
    <pubDate>Fri, 17 Nov 2023 01:53:55 GMT</pubDate>
    <dc:creator>shiqi_seventeen</dc:creator>
    <dc:date>2023-11-17T01:53:55Z</dc:date>
    <item>
      <title>FS2633 WAKE UP</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS2633-WAKE-UP/m-p/1758697#M20135</link>
      <description>&lt;P&gt;Hello Team, I am using FS2633, there are three questions about FS26 LPOFF mode wake-up :&lt;BR /&gt;FS26 LPOFF mode wake-up issue, 0x57 register read value=0x2009:&lt;BR /&gt;1: Power on to call Sbc_ Fs26_ The SetOperatingMode function allows you to enter LPOFF mode normally.&lt;BR /&gt;2: After powering on and operating other registers, call Sbc again_ Fs26_ The SetOperatingMode function is invalid when it enters LPOFF. (CRC verification is normal, and the oscilloscope has checked that there is no fluctuation in the output voltage.)&lt;BR /&gt;3: In debug mode, clearing the wake-up source and configuring the wake-up source ensures that the wake-up source is currently at a low level,&lt;BR /&gt;Call Sbc again_ Fs26_ SetOperatingMode failed to enter LPOFF mode, and the output voltage was checked through an oscilloscope without any fluctuations.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Nov 2023 01:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS2633-WAKE-UP/m-p/1758697#M20135</guid>
      <dc:creator>shiqi_seventeen</dc:creator>
      <dc:date>2023-11-17T01:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: FS2633 WAKE UP</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS2633-WAKE-UP/m-p/1759635#M20159</link>
      <description>&lt;P&gt;目前您这边面临的问题是什么？麻烦详细的描述出来多谢！&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 07:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS2633-WAKE-UP/m-p/1759635#M20159</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-11-20T07:19:53Z</dc:date>
    </item>
  </channel>
</rss>