<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Using QSPI1 as normal SPI MC56F84786</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Using-QSPI1-as-normal-SPI-MC56F84786/m-p/1752622#M19965</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The spi of MC56F84786 is called queued spi instead of quad spi. The QSPI of MC56F84xxx is a normal spi interface,it can interface with 4 pins spi flash, the 4 pins includes sck, /cs, mosi and miso.&lt;/P&gt;
&lt;P&gt;Obviously, it can not interface with quad spi flash.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 06 Nov 2023 08:12:01 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-11-06T08:12:01Z</dc:date>
    <item>
      <title>Using QSPI1 as normal SPI MC56F84786</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Using-QSPI1-as-normal-SPI-MC56F84786/m-p/1750503#M19899</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;Dear Mr. and Mrs.,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I have a board with MC56F84786 NXP microcontroller. This MCU is connected with Flash memory via SPI. In addition to this, Flash has QSPI pins but in this design, QSPI pins are not used. Instead of QSPI pins, SPI pins are used. I saw configuration for QSPI on IDE. I couldn’t see config for SPI. QSPI1 could be used as standard SPI . Is Library of QSPI1 valid for SPI. How should be config for SPI by using QSPI1 on Codewarrior?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Thanks in advance for supports.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;Sidar&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Nov 2023 07:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Using-QSPI1-as-normal-SPI-MC56F84786/m-p/1750503#M19899</guid>
      <dc:creator>20Sidar04</dc:creator>
      <dc:date>2023-11-02T07:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: Using QSPI1 as normal SPI MC56F84786</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Using-QSPI1-as-normal-SPI-MC56F84786/m-p/1752622#M19965</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The spi of MC56F84786 is called queued spi instead of quad spi. The QSPI of MC56F84xxx is a normal spi interface,it can interface with 4 pins spi flash, the 4 pins includes sck, /cs, mosi and miso.&lt;/P&gt;
&lt;P&gt;Obviously, it can not interface with quad spi flash.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 08:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Using-QSPI1-as-normal-SPI-MC56F84786/m-p/1752622#M19965</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-11-06T08:12:01Z</dc:date>
    </item>
  </channel>
</rss>