<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPCA9518</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752334#M19958</link>
    <description>&lt;P&gt;I am facing a weird issue, I am connecting ATMEGA128 (running on 5v VCC) to PCA9518 through TSX0102 for both SCL &amp;amp; SDA lines. the PCA9518 is included to buffer I2C communication between ATMEGA128 and four other boards. The SCL0 &amp;amp; SDA0 are 3.3v, while all other ports are 5v (&lt;SPAN&gt;pull-up resistors connected to 5v). SCL signal can be seen on all ports, but with lower frequency than targeted (66.2KHz instead&amp;nbsp;of 100KHz) and SDA is always zero logic on all port no matter&amp;nbsp;which one is enabled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am suspecting the cause to be one of the following:&lt;/P&gt;&lt;P&gt;1. Using PCA9518 in series with &lt;SPAN&gt;TSX0102&amp;nbsp;rise time accelerator which might be incompatible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. Using large bypass capacitors connected to VCC (3.3V) one 10 uF tantalum in parallel with 0.1 uF MLCC.&lt;/P&gt;&lt;P&gt;3. Connecting EXPSCL1&amp;amp;2 EXPSDA1&amp;amp;2 pull-up resistors to 5V.&lt;/P&gt;&lt;P&gt;4. Connecting all EN to 5v logic signals.&lt;/P&gt;&lt;P&gt;5. Not connecting extra pull-ups at the&amp;nbsp;&lt;SPAN&gt;TSX0102&amp;nbsp;outputs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;attached is part of the schematic regarding this point.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please can anyone assist in diagnosing the cause of the&amp;nbsp;issue.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 05 Nov 2023 12:53:41 GMT</pubDate>
    <dc:creator>AbdallaDawoud</dc:creator>
    <dc:date>2023-11-05T12:53:41Z</dc:date>
    <item>
      <title>PCA9518</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752334#M19958</link>
      <description>&lt;P&gt;I am facing a weird issue, I am connecting ATMEGA128 (running on 5v VCC) to PCA9518 through TSX0102 for both SCL &amp;amp; SDA lines. the PCA9518 is included to buffer I2C communication between ATMEGA128 and four other boards. The SCL0 &amp;amp; SDA0 are 3.3v, while all other ports are 5v (&lt;SPAN&gt;pull-up resistors connected to 5v). SCL signal can be seen on all ports, but with lower frequency than targeted (66.2KHz instead&amp;nbsp;of 100KHz) and SDA is always zero logic on all port no matter&amp;nbsp;which one is enabled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am suspecting the cause to be one of the following:&lt;/P&gt;&lt;P&gt;1. Using PCA9518 in series with &lt;SPAN&gt;TSX0102&amp;nbsp;rise time accelerator which might be incompatible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. Using large bypass capacitors connected to VCC (3.3V) one 10 uF tantalum in parallel with 0.1 uF MLCC.&lt;/P&gt;&lt;P&gt;3. Connecting EXPSCL1&amp;amp;2 EXPSDA1&amp;amp;2 pull-up resistors to 5V.&lt;/P&gt;&lt;P&gt;4. Connecting all EN to 5v logic signals.&lt;/P&gt;&lt;P&gt;5. Not connecting extra pull-ups at the&amp;nbsp;&lt;SPAN&gt;TSX0102&amp;nbsp;outputs.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;attached is part of the schematic regarding this point.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please can anyone assist in diagnosing the cause of the&amp;nbsp;issue.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 05 Nov 2023 12:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752334#M19958</guid>
      <dc:creator>AbdallaDawoud</dc:creator>
      <dc:date>2023-11-05T12:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9518</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752349#M19959</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;It's possible that the 3.3V SCL signal affects PCA9518. Try using a level shifter for 5V compatibility. Check connections thoroughly.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Sun, 05 Nov 2023 19:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752349#M19959</guid>
      <dc:creator>MarkChapman</dc:creator>
      <dc:date>2023-11-05T19:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9518</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752556#M19963</link>
      <description>&lt;P&gt;Please share with your schematic here.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 07:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752556#M19963</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-11-06T07:05:07Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9518</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752856#M19976</link>
      <description>&lt;P&gt;Thanks Mark l, you were right. After careful connections checking again for the third time, it turned out that one of EXPSDA’s pull-up resistor was not properly soldered, having it well-soldered has resolved the issue completely.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 13:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9518/m-p/1752856#M19976</guid>
      <dc:creator>AbdallaDawoud</dc:creator>
      <dc:date>2023-11-06T13:36:54Z</dc:date>
    </item>
  </channel>
</rss>