<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: PCA21125 RTC Get real time</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1751156#M19919</link>
    <description>Thank you for suggesting me the UM10301 user manual. As given in the module, chapter 12.1 table 5 I need to initialize the RTC POR bit of Control register 1 and RF bit of Second register should be cleared. But I am facing issue while clearing POR bit of Control Register 1 and RF bit of Second Register. I am not able to clear these above bits. How can I resolve this issue ?</description>
    <pubDate>Thu, 02 Nov 2023 12:58:15 GMT</pubDate>
    <dc:creator>AshBirari</dc:creator>
    <dc:date>2023-11-02T12:58:15Z</dc:date>
    <item>
      <title>PCA21125 RTC Get real time</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1750801#M19907</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I am trying to get the real time using RTC PCA21125.Following way I have implemented the RTC interface with AURIX TC389 controller using SPI communication.&lt;/P&gt;&lt;P&gt;Write Command : 0x10&lt;/P&gt;&lt;P&gt;Read Command : 0x90&lt;/P&gt;&lt;P&gt;SPI Configurations&amp;nbsp; :&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Data width : 8&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Transfer Start : MSB&lt;/P&gt;&lt;P&gt;RTC Initialization :&lt;/P&gt;&lt;P&gt;Configuring Register Control 1 as 0x0C (POR_OVRD = 1, 12_24 = 1)[is this correct way ?]&lt;/P&gt;&lt;P&gt;&amp;nbsp;Configuring Register Control 1 as 0x00&lt;/P&gt;&lt;P&gt;RF bit of SECOND regirster is always 1 as its default value.&lt;/P&gt;&lt;P&gt;trying to read the Second, Minute, Hour data from the register using SPI commands.&lt;/P&gt;&lt;P&gt;Observed&amp;nbsp; Values :&lt;/P&gt;&lt;P&gt;Seconds :&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;Minutes : 19&lt;/P&gt;&lt;P&gt;Hours : 12&lt;/P&gt;</description>
      <pubDate>Thu, 02 Nov 2023 12:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1750801#M19907</guid>
      <dc:creator>AshBirari</dc:creator>
      <dc:date>2023-11-02T12:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: PCA21125 RTC Get real time</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1751140#M19916</link>
      <description>&lt;P&gt;Hello Ashwini,&lt;/P&gt;
&lt;P&gt;I do not fully understand what is the issue you are facing.&lt;/P&gt;
&lt;P&gt;I would recommend you to take a closer look at our &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10301.pdf" target="_self"&gt;UM10301&lt;/A&gt;, mainly chapters 12.1&amp;nbsp; - Initialization of the RTC and setting the time, and 6 - Oscillator.&lt;/P&gt;
&lt;P&gt;The simplest way to check for oscillation is to use the CLKOUT pin. There should be a 32.768 kHz signal at pin CLKOUT available after power-on. If your design does not include a pull-up resistor to the CLKOUT, then add one temporarily.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 02 Nov 2023 12:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1751140#M19916</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-11-02T12:38:40Z</dc:date>
    </item>
    <item>
      <title>Re: PCA21125 RTC Get real time</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1751156#M19919</link>
      <description>Thank you for suggesting me the UM10301 user manual. As given in the module, chapter 12.1 table 5 I need to initialize the RTC POR bit of Control register 1 and RF bit of Second register should be cleared. But I am facing issue while clearing POR bit of Control Register 1 and RF bit of Second Register. I am not able to clear these above bits. How can I resolve this issue ?</description>
      <pubDate>Thu, 02 Nov 2023 12:58:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA21125-RTC-Get-real-time/m-p/1751156#M19919</guid>
      <dc:creator>AshBirari</dc:creator>
      <dc:date>2023-11-02T12:58:15Z</dc:date>
    </item>
  </channel>
</rss>