<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピックntb0102</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726027#M19318</link>
    <description>&lt;P&gt;I would like to use NTB0102 for level conversion (3.3V⇔5.0V) for the SDI-12 interface. The speed is 1200bps. Since we want the voltage to be 0V at startup, we will attach a pull-down resistor to the A side. Please use twisted pair wires with a cable length of approximately 2 to 3 meters. NTB0102 is equipped with a 2-bit level conversion circuit, but only 1 bit is used. Connect unused pins to 0V.&lt;BR /&gt;1. Can I use NTB0102?&lt;BR /&gt;2. Is there a 1-bit version of the NTB010x series?&lt;BR /&gt;3. Please tell me how to calculate the pull-down resistance value.&lt;/P&gt;</description>
    <pubDate>Wed, 20 Sep 2023 07:26:31 GMT</pubDate>
    <dc:creator>Satake</dc:creator>
    <dc:date>2023-09-20T07:26:31Z</dc:date>
    <item>
      <title>ntb0102</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726027#M19318</link>
      <description>&lt;P&gt;I would like to use NTB0102 for level conversion (3.3V⇔5.0V) for the SDI-12 interface. The speed is 1200bps. Since we want the voltage to be 0V at startup, we will attach a pull-down resistor to the A side. Please use twisted pair wires with a cable length of approximately 2 to 3 meters. NTB0102 is equipped with a 2-bit level conversion circuit, but only 1 bit is used. Connect unused pins to 0V.&lt;BR /&gt;1. Can I use NTB0102?&lt;BR /&gt;2. Is there a 1-bit version of the NTB010x series?&lt;BR /&gt;3. Please tell me how to calculate the pull-down resistance value.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 07:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726027#M19318</guid>
      <dc:creator>Satake</dc:creator>
      <dc:date>2023-09-20T07:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: ntb0102</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726838#M19332</link>
      <description>&lt;P&gt;Hi Satake,&lt;/P&gt;
&lt;P data-unlink="true"&gt;Yes, we do have a 1-bit version of the NTB010x series - &lt;A href="https://www.nxp.com/products/peripherals-and-logic/voltage-level-translators/dual-supply-translating-transceiver-auto-direction-sensing-three-state:NTB0101" target="_self"&gt;NTB0101&lt;/A&gt;&amp;nbsp;which you can use for level conversion between 3.3V and 5.0V for your SDI-12 interface running at 1200bps.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would recommend to choose a pull-down resistor of approximately 2.5k ohms.&lt;/P&gt;
&lt;P&gt;BR, Tomas&lt;/P&gt;
&lt;P data-unlink="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 06:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726838#M19332</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-09-21T06:47:12Z</dc:date>
    </item>
    <item>
      <title>Re: ntb0102</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726927#M19334</link>
      <description>&lt;P&gt;Hi.Tomas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you. I'll buy it right away and check it out. It was helpful.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 07:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ntb0102/m-p/1726927#M19334</guid>
      <dc:creator>Satake</dc:creator>
      <dc:date>2023-09-21T07:59:12Z</dc:date>
    </item>
  </channel>
</rss>