<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックTJA1145A Power Sequence Issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145A-Power-Sequence-Issue/m-p/1724913#M19297</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am experiencing an issue when debugging a board using the TJA1145AT. Normal operation brings on VBAT before VCC or VIO, but I found when using a debugger for the microprocessor, VIO was powered via the debugger without VBAT and VCC powered. After this happens, the board stops working, and it seems like the TJA1145AT is damaged. I can still talk to the microprocessor via debugger (successful programming and reading out memories).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to damage the TJA1145AT if VIO is powered without VBAT and VCC?&lt;/P&gt;</description>
    <pubDate>Mon, 18 Sep 2023 18:59:14 GMT</pubDate>
    <dc:creator>lmb_bruker</dc:creator>
    <dc:date>2023-09-18T18:59:14Z</dc:date>
    <item>
      <title>TJA1145A Power Sequence Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145A-Power-Sequence-Issue/m-p/1724913#M19297</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am experiencing an issue when debugging a board using the TJA1145AT. Normal operation brings on VBAT before VCC or VIO, but I found when using a debugger for the microprocessor, VIO was powered via the debugger without VBAT and VCC powered. After this happens, the board stops working, and it seems like the TJA1145AT is damaged. I can still talk to the microprocessor via debugger (successful programming and reading out memories).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to damage the TJA1145AT if VIO is powered without VBAT and VCC?&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 18:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1145A-Power-Sequence-Issue/m-p/1724913#M19297</guid>
      <dc:creator>lmb_bruker</dc:creator>
      <dc:date>2023-09-18T18:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1145A Power Sequence Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145A-Power-Sequence-Issue/m-p/1727491#M19346</link>
      <description>&lt;P&gt;I don't think it will damage if VIO powered without Vbat and Vcc, but you need pay attention on the limited value once above this max 6V it will damage:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_0-1695340949113.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/242108iF22B5C5574793127/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_0-1695340949113.png" alt="guoweisun_0-1695340949113.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_0-1695340949113.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 00:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1145A-Power-Sequence-Issue/m-p/1727491#M19346</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-09-22T00:02:54Z</dc:date>
    </item>
  </channel>
</rss>