<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: PCA9955B Short Circuit Detection Issues</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713489#M19109</link>
    <description>&lt;P&gt;Thank you for the response, please see attached for an image of the relevant part of my schematic.&lt;/P&gt;&lt;P&gt;I don't have the unused outputs tied to Vdd through that resistor - but would that be causing a short error in LEDs that are there?&lt;/P&gt;&lt;P&gt;I can add the LED in the coming days and keep you posted as well.&lt;/P&gt;</description>
    <pubDate>Tue, 29 Aug 2023 20:36:34 GMT</pubDate>
    <dc:creator>ricola96</dc:creator>
    <dc:date>2023-08-29T20:36:34Z</dc:date>
    <item>
      <title>PCA9955B Short Circuit Detection Issues</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713297#M19104</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've got a design that uses the PCA9955B and I'm having issues where there is a short circuit reported on all LEDs.&lt;/P&gt;&lt;P&gt;I measure the input pins of the driver and I'm reading ~3.4V but I noticed in the datasheet that if Vo &amp;gt;= Vth then the short circuit error happens. Vth is ~2.85V as per the datasheet.&lt;/P&gt;&lt;P&gt;I'm controlling my LEDs with 5V - is the intention that the LED is used to drop that 5V to something &amp;lt; 2.85V?&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 13:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713297#M19104</guid>
      <dc:creator>ricola96</dc:creator>
      <dc:date>2023-08-29T13:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9955B Short Circuit Detection Issues</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713468#M19107</link>
      <description>&lt;P&gt;Hello, could you please share your schematic?&lt;/P&gt;
&lt;P&gt;Remember that for all unused LED outputs, the user must program their LED outputs to the ‘OFF’ state (LDRx = 00) and IREFx value to 00h, and all unused LED output pins must be pulled up to VDD with a recommended 100 k shared resistor.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 19:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713468#M19107</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-08-29T19:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9955B Short Circuit Detection Issues</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713489#M19109</link>
      <description>&lt;P&gt;Thank you for the response, please see attached for an image of the relevant part of my schematic.&lt;/P&gt;&lt;P&gt;I don't have the unused outputs tied to Vdd through that resistor - but would that be causing a short error in LEDs that are there?&lt;/P&gt;&lt;P&gt;I can add the LED in the coming days and keep you posted as well.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 20:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9955B-Short-Circuit-Detection-Issues/m-p/1713489#M19109</guid>
      <dc:creator>ricola96</dc:creator>
      <dc:date>2023-08-29T20:36:34Z</dc:date>
    </item>
  </channel>
</rss>