<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C PCA9601 and PCA9548A 8ch mux in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1702773#M18877</link>
    <description>&lt;P&gt;Thanks for confirming&lt;/P&gt;</description>
    <pubDate>Thu, 10 Aug 2023 08:22:42 GMT</pubDate>
    <dc:creator>Henkk</dc:creator>
    <dc:date>2023-08-10T08:22:42Z</dc:date>
    <item>
      <title>I2C PCA9601 and PCA9548A 8ch mux</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1701984#M18862</link>
      <description>&lt;P&gt;The datasheet of the PCA9601 section 7.3 say: "Two or more SX or SY I/Os must not be interconnected. The PCA9601 design does not support this configuration. Bidirectional I2C-bus signals do not allow any direction control pin so, instead, slightly different logic LOW voltage levels are used at SX/SY to avoid latching of this buffer . . . . . . . ."&lt;/P&gt;&lt;P&gt;The question is: Is it possible to connect a PCA9548 8ch mux (SDA pin 23 and SCL pin 22 on TSSOP package) to the SX and SY pins of the PCA9601.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The PCA9548 is not a bus buffer, but has mosfets to connect a channel to the I2C bus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help or clarification would be much appreciated&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 13:37:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1701984#M18862</guid>
      <dc:creator>Henkk</dc:creator>
      <dc:date>2023-08-09T13:37:19Z</dc:date>
    </item>
    <item>
      <title>Re: I2C PCA9601 and PCA9548A 8ch mux</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1702209#M18867</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Yes, you can connect&amp;nbsp;&lt;SPAN&gt;PCA9548&amp;nbsp;SDA pin and SCL pin to the SX and SY pins of the PCA9601.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 18:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1702209#M18867</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-08-09T18:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: I2C PCA9601 and PCA9548A 8ch mux</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1702773#M18877</link>
      <description>&lt;P&gt;Thanks for confirming&lt;/P&gt;</description>
      <pubDate>Thu, 10 Aug 2023 08:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1702773#M18877</guid>
      <dc:creator>Henkk</dc:creator>
      <dc:date>2023-08-10T08:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: I2C PCA9601 and PCA9548A 8ch mux</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1706502#M18973</link>
      <description>Got a prototype working, I use the PCA9601 to connect I2C over RS422 and use Cat5e. I've tested it up to 266 meter (I didn't have more cable at the time)</description>
      <pubDate>Thu, 17 Aug 2023 09:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-PCA9601-and-PCA9548A-8ch-mux/m-p/1706502#M18973</guid>
      <dc:creator>Henkk</dc:creator>
      <dc:date>2023-08-17T09:32:03Z</dc:date>
    </item>
  </channel>
</rss>