<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TJA1153 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699894#M18823</link>
    <description>&lt;P&gt;Hi, thanks for the reply.&lt;/P&gt;&lt;P&gt;We are looking into the secured transceivers. However, per 1153 datasheet seems that can support arbitration rate of up to 500 Kbps and not 1 Mbps&lt;/P&gt;&lt;P&gt;• Operates in Classical CAN and CAN FD systems with arbitration phase bit rate set at&lt;BR /&gt;125 kbit/s, 250 kbit/s or 500 kbit/s&lt;/P&gt;&lt;P&gt;(also per CAN_CANFD_BR settings)&lt;/P&gt;&lt;P&gt;In NXP roadmap - is there intension to support 1 Mbps of arbitration rate?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;• For arbitration bit rates of 250 kbit/s and 500 kbit/s, the fast phase bit rate can be set to&lt;BR /&gt;two or four times the arbitration bit rate&lt;/P&gt;</description>
    <pubDate>Mon, 07 Aug 2023 05:45:29 GMT</pubDate>
    <dc:creator>YoavBarY</dc:creator>
    <dc:date>2023-08-07T05:45:29Z</dc:date>
    <item>
      <title>TJA1153</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1698375#M18783</link>
      <description>&lt;P&gt;The TJA1153 supports 500Kb according to the datasheet&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a secure CAN Transceiver that supports 1Mb? If not, Is there a roadmap for pin compatible device that is a secure CAN transceiver up to 1Mb?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 07:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1698375#M18783</guid>
      <dc:creator>raztiko</dc:creator>
      <dc:date>2023-08-03T07:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1698455#M18788</link>
      <description>&lt;P&gt;Dear Raz,&lt;/P&gt;
&lt;P&gt;for our CAN transceivers portfolio please refer to this &lt;A href="https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR?category=c704_c707" target="_self"&gt;link&lt;/A&gt;. The TJA1153A supports data rate up to 5Mbit/s.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1691052163342.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/234929i29278D056671F2BA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1691052163342.png" alt="JozefKozon_0-1691052163342.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 08:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1698455#M18788</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-08-03T08:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699723#M18820</link>
      <description>&lt;P&gt;Hi, thanks for the reply.&lt;/P&gt;&lt;P&gt;We are looking into the secured transceivers. However, per 1153 datasheet seems that can support arbitration rate of up to 500 Kbps and not 1 Mbps&lt;/P&gt;&lt;P&gt;• Operates in Classical CAN and CAN FD systems with arbitration phase bit rate set at&lt;BR /&gt;125 kbit/s, 250 kbit/s or 500 kbit/s&lt;/P&gt;&lt;P&gt;(also per CAN_CANFD_BR settings)&lt;/P&gt;&lt;P&gt;In NXP roadmap - is there intension to support 1 Mbps of arbitration rate?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;• For arbitration bit rates of 250 kbit/s and 500 kbit/s, the fast phase bit rate can be set to&lt;BR /&gt;two or four times the arbitration bit rate&lt;/P&gt;</description>
      <pubDate>Sun, 06 Aug 2023 14:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699723#M18820</guid>
      <dc:creator>YoavBY</dc:creator>
      <dc:date>2023-08-06T14:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699894#M18823</link>
      <description>&lt;P&gt;Hi, thanks for the reply.&lt;/P&gt;&lt;P&gt;We are looking into the secured transceivers. However, per 1153 datasheet seems that can support arbitration rate of up to 500 Kbps and not 1 Mbps&lt;/P&gt;&lt;P&gt;• Operates in Classical CAN and CAN FD systems with arbitration phase bit rate set at&lt;BR /&gt;125 kbit/s, 250 kbit/s or 500 kbit/s&lt;/P&gt;&lt;P&gt;(also per CAN_CANFD_BR settings)&lt;/P&gt;&lt;P&gt;In NXP roadmap - is there intension to support 1 Mbps of arbitration rate?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;• For arbitration bit rates of 250 kbit/s and 500 kbit/s, the fast phase bit rate can be set to&lt;BR /&gt;two or four times the arbitration bit rate&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 05:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699894#M18823</guid>
      <dc:creator>YoavBarY</dc:creator>
      <dc:date>2023-08-07T05:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1153</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699963#M18826</link>
      <description>&lt;P&gt;Hi Raz,&lt;/P&gt;
&lt;P&gt;I apologize, I misunderstood you. Unfortunately no. We do not have a CAN transceiver with Arbitration rate of 1Mbit/s and there is not any planned. I apologize for inconvenience.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 07:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1153/m-p/1699963#M18826</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-08-07T07:02:10Z</dc:date>
    </item>
  </channel>
</rss>