<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックMR-T1ETH8 FAQ</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MR-T1ETH8-FAQ/m-p/1699439#M18814</link>
    <description>&lt;P&gt;While MR-T1ETH8 was developed for integration with other mobile robotics solutions/reference boards such as NavQPlus, FMUK66, MR-VMU-RT1176, RDDRONE-T1ADAPT, MR-CANHUBK344, the mobile robotics team does find a lot of non- mobile robotics customers are using it for various purposes.&lt;BR /&gt;&lt;BR /&gt;This is an informal attempt at an FAQ for this board:&lt;BR /&gt;-=-=-=-=-&lt;BR /&gt;Q: Where can i get software support for developing on this board?&lt;BR /&gt;A: Currently the&amp;nbsp;T1ETH8 is a hardware reference only. For any software development, you must also refer to the SJA1110 EVK from the Automotive Business line. You can expect that Automotive customers will get priority.&amp;nbsp; Support will only be in reference the SJA1110 EVK and not the MR-T1ETH8&lt;/P&gt;&lt;P&gt;Of course any software developed on the EVK will also run on this hardware reference.&lt;/P&gt;&lt;P&gt;-=-=-=-=-&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there an SDK we can use to develop our own product based on the MR-T1ETH8? We requested the secured files but the SDK referred to on the webpage was not included.&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The code is developed with S32DS version 3.4 and the SJA1110 SDK.&lt;/LI&gt;&lt;LI&gt;Sources are internally available (collabnet) and may be available if requested through the automotive networking BL.&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Is the edge lock chip mandatory to use with this design?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The use case enabled is as NFC interface to an Android mobile phone app. This is NOT based on any SDK.&lt;/LI&gt;&lt;LI&gt;For the switch use case this is not a requirement&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;What is the switch’s default configuration?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The default code just supports the switch as a switch.&lt;/LI&gt;&lt;LI&gt;The idea here is that tftp can be used to upload new firmware to enable more features.&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Does the switch have VLAN capabilities enabled by default? If not, what steps are needed to enable VLAN support?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;No just plain switch&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Is there any type of active feedback/communication between the switch and the PMIC?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;No communication to the PMIC&lt;/LI&gt;&lt;/UL&gt;&lt;/OL&gt;</description>
    <pubDate>Fri, 04 Aug 2023 13:46:20 GMT</pubDate>
    <dc:creator>iaingalloway</dc:creator>
    <dc:date>2023-08-04T13:46:20Z</dc:date>
    <item>
      <title>MR-T1ETH8 FAQ</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MR-T1ETH8-FAQ/m-p/1699439#M18814</link>
      <description>&lt;P&gt;While MR-T1ETH8 was developed for integration with other mobile robotics solutions/reference boards such as NavQPlus, FMUK66, MR-VMU-RT1176, RDDRONE-T1ADAPT, MR-CANHUBK344, the mobile robotics team does find a lot of non- mobile robotics customers are using it for various purposes.&lt;BR /&gt;&lt;BR /&gt;This is an informal attempt at an FAQ for this board:&lt;BR /&gt;-=-=-=-=-&lt;BR /&gt;Q: Where can i get software support for developing on this board?&lt;BR /&gt;A: Currently the&amp;nbsp;T1ETH8 is a hardware reference only. For any software development, you must also refer to the SJA1110 EVK from the Automotive Business line. You can expect that Automotive customers will get priority.&amp;nbsp; Support will only be in reference the SJA1110 EVK and not the MR-T1ETH8&lt;/P&gt;&lt;P&gt;Of course any software developed on the EVK will also run on this hardware reference.&lt;/P&gt;&lt;P&gt;-=-=-=-=-&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there an SDK we can use to develop our own product based on the MR-T1ETH8? We requested the secured files but the SDK referred to on the webpage was not included.&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The code is developed with S32DS version 3.4 and the SJA1110 SDK.&lt;/LI&gt;&lt;LI&gt;Sources are internally available (collabnet) and may be available if requested through the automotive networking BL.&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Is the edge lock chip mandatory to use with this design?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The use case enabled is as NFC interface to an Android mobile phone app. This is NOT based on any SDK.&lt;/LI&gt;&lt;LI&gt;For the switch use case this is not a requirement&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;What is the switch’s default configuration?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;The default code just supports the switch as a switch.&lt;/LI&gt;&lt;LI&gt;The idea here is that tftp can be used to upload new firmware to enable more features.&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Does the switch have VLAN capabilities enabled by default? If not, what steps are needed to enable VLAN support?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;No just plain switch&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;Is there any type of active feedback/communication between the switch and the PMIC?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;No communication to the PMIC&lt;/LI&gt;&lt;/UL&gt;&lt;/OL&gt;</description>
      <pubDate>Fri, 04 Aug 2023 13:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MR-T1ETH8-FAQ/m-p/1699439#M18814</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2023-08-04T13:46:20Z</dc:date>
    </item>
  </channel>
</rss>