<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Communication between SJA1124 and Raspberry PI</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1697403#M18755</link>
    <description>&lt;P&gt;Hello Erica, thanks you for responding.&lt;BR /&gt;So you will find the signals SCK, SDI and the CLK ,concerning VDD I checked it's 3.3V, as for&amp;nbsp;&lt;SPAN&gt;P3V3 and P5V0 they are both 0V&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Aug 2023 08:43:56 GMT</pubDate>
    <dc:creator>Khaled_tn</dc:creator>
    <dc:date>2023-08-02T08:43:56Z</dc:date>
    <item>
      <title>Communication between SJA1124 and Raspberry PI</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1696716#M18728</link>
      <description>&lt;P&gt;Hello, I am trying to send SPI frames to the evaluation board&amp;nbsp;SJA1124EVB from my raspberry PI, I followed the Quick Start Guide of the board and I :&lt;BR /&gt;- Powered the board with 12V&lt;BR /&gt;- Made all the necessary SPI wiring(SCK, SDO, SDI,&amp;nbsp;SPI chip select input #0)&lt;BR /&gt;- Provided a 2MHz clock for the board from an external oscillator&lt;BR /&gt;-Send SPI frames for the board using the software&amp;nbsp;NXP_SJA1124_Example_App provided in the NXP website(&lt;SPAN&gt;SJA1124_Init,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Lin_Init,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SJA1124_GetStatus, ...)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;when running the script my oscilloscope shows the frames in SDI, also shows a normal functionning of the L_INH0, a normal SCK but I for the SDO I am receinving a weird signal (not noise) as if it is not in the good level or not enough&amp;nbsp; amplified.&lt;BR /&gt;You can find the signal SDO received.&lt;BR /&gt;Can you help to figure out what I may forgot or what could be wrong ?&lt;BR /&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Aug 2023 12:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1696716#M18728</guid>
      <dc:creator>Khaled_tn</dc:creator>
      <dc:date>2023-08-01T12:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between SJA1124 and Raspberry PI</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1696926#M18740</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you attach a picture of your oscilloscope with the clock signal and the SDI signal, as well as you could check that there is VDD voltage (3.3V / 5V), P3V3 (3.3V) and P5V0 (5V) as reference voltages, to check the operation of the board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Aug 2023 18:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1696926#M18740</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-08-01T18:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between SJA1124 and Raspberry PI</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1697403#M18755</link>
      <description>&lt;P&gt;Hello Erica, thanks you for responding.&lt;BR /&gt;So you will find the signals SCK, SDI and the CLK ,concerning VDD I checked it's 3.3V, as for&amp;nbsp;&lt;SPAN&gt;P3V3 and P5V0 they are both 0V&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 08:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1697403#M18755</guid>
      <dc:creator>Khaled_tn</dc:creator>
      <dc:date>2023-08-02T08:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between SJA1124 and Raspberry PI</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1697921#M18767</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;You should measure&amp;nbsp;P3V3 (3.3V) and P5V0 (5V).&amp;nbsp;Otherwise, SJA1124 and other components on the boards can be damaged. Do you have another SJA1124EVB to check it? Because I do not see errors with the signals and the steps you are following.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 02 Aug 2023 18:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1697921#M18767</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-08-02T18:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: Communication between SJA1124 and Raspberry PI</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1698778#M18801</link>
      <description>&lt;P&gt;Hello again,&lt;BR /&gt;&lt;BR /&gt;I realized that I had to apply a 3.3V in the VDD (J3-2) pin to the board, even though I had already measured 3.3V in it.&amp;nbsp;&lt;BR /&gt;That made me get response to my SPI frames that I've sent, although the frames I am receiving are identical to the ones I am sending even when calling "&lt;SPAN&gt;SJA1124_GetStatus"&amp;nbsp;&lt;/SPAN&gt;function that reads the Interruptions registers.&lt;/P&gt;&lt;P&gt;for example, after calling the&amp;nbsp;&lt;FONT face="inherit"&gt;SJA1124_Init, I've sent the frame {0x10, 0x83, 0, 0, 0, 0} to read the &lt;/FONT&gt;interruptions&lt;FONT face="inherit"&gt;&amp;nbsp;&amp;nbsp;registers I've received the Identical frame from the SDO pin from the board. (Image attached)&amp;nbsp; &amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Do you have any idea haw should normally the board responds to the SPI frames (through the SDO pin)?&lt;BR /&gt;Thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Aug 2023 15:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-between-SJA1124-and-Raspberry-PI/m-p/1698778#M18801</guid>
      <dc:creator>Khaled_tn</dc:creator>
      <dc:date>2023-08-03T15:54:57Z</dc:date>
    </item>
  </channel>
</rss>