<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックMFRC630 - RxN/RxP Signals</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MFRC630-RxN-RxP-Signals/m-p/1695135#M18681</link>
    <description>&lt;P&gt;I'm currently working on a RFID Reader that uses the MFRC630 and CLRC663. Also i have a fully working prototype with matched antenna that works very well with different tags, sizes and distances.&lt;/P&gt;&lt;P&gt;Currently I'm stuck at finding the correct External Rx Components.&lt;/P&gt;&lt;P&gt;In AN11019 in Section 4.4.1 there is described to elect R2A and R2B from a starting value (i used 15k) and increase the resistance to get a Signal that is &amp;lt;=1.7V and &amp;gt;=1.2V&lt;/P&gt;&lt;P&gt;But in my case, changing the resistance does not affect the voltage a lot, from 15k where my Umax was around 2.3V i changed to 27k and now to 39k. Currently Umax is 1.73V and Upp is 1.55V. The change between 27k and 39k the voltage only decreased around 100mV.&lt;/P&gt;&lt;P&gt;Attached is a scope shot of the signal with a passive probe that has 4pF (currently no active probe available). Can the probe be the problem? Do i have a faulty IC? Is it possible that i have to increase the resistance even more?&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jul 2023 16:12:58 GMT</pubDate>
    <dc:creator>jof_tcs</dc:creator>
    <dc:date>2023-07-28T16:12:58Z</dc:date>
    <item>
      <title>MFRC630 - RxN/RxP Signals</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MFRC630-RxN-RxP-Signals/m-p/1695135#M18681</link>
      <description>&lt;P&gt;I'm currently working on a RFID Reader that uses the MFRC630 and CLRC663. Also i have a fully working prototype with matched antenna that works very well with different tags, sizes and distances.&lt;/P&gt;&lt;P&gt;Currently I'm stuck at finding the correct External Rx Components.&lt;/P&gt;&lt;P&gt;In AN11019 in Section 4.4.1 there is described to elect R2A and R2B from a starting value (i used 15k) and increase the resistance to get a Signal that is &amp;lt;=1.7V and &amp;gt;=1.2V&lt;/P&gt;&lt;P&gt;But in my case, changing the resistance does not affect the voltage a lot, from 15k where my Umax was around 2.3V i changed to 27k and now to 39k. Currently Umax is 1.73V and Upp is 1.55V. The change between 27k and 39k the voltage only decreased around 100mV.&lt;/P&gt;&lt;P&gt;Attached is a scope shot of the signal with a passive probe that has 4pF (currently no active probe available). Can the probe be the problem? Do i have a faulty IC? Is it possible that i have to increase the resistance even more?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jul 2023 16:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MFRC630-RxN-RxP-Signals/m-p/1695135#M18681</guid>
      <dc:creator>jof_tcs</dc:creator>
      <dc:date>2023-07-28T16:12:58Z</dc:date>
    </item>
  </channel>
</rss>