<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046 TMU clock config in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046-TMU-clock-config/m-p/1689041#M18518</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220462"&gt;@yirw&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;A given application may not use all the peripherals on the device. In that case, it may be desirable to disable unused peripherals. DEVDISR provides a mechanism for gating clocks to IP blocks that are not used when running an application. &lt;BR /&gt;You can enable/disable the TMU monitoring mode by configuring TMR[ME] mode bit. Please refer to chapter# 33 in the LS1046ARM for more details.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jul 2023 06:45:02 GMT</pubDate>
    <dc:creator>mrudangshelat-13</dc:creator>
    <dc:date>2023-07-20T06:45:02Z</dc:date>
    <item>
      <title>LS1046 TMU clock config</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046-TMU-clock-config/m-p/1688801#M18513</link>
      <description>&lt;P&gt;In the LS146ARM Clocking chapter, the clock for TMU is 1/2 Platform Clock. Clock enablements such as spi, i2c, gpio, etc. are configured in the DEVDISR register of Chapter 12 “Device Configuration and Pin Control”, but no TMU related configuration bit is found. How should the TMU clock be configured? Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 03:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046-TMU-clock-config/m-p/1688801#M18513</guid>
      <dc:creator>yirw</dc:creator>
      <dc:date>2023-07-20T03:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 TMU clock config</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046-TMU-clock-config/m-p/1689041#M18518</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220462"&gt;@yirw&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;A given application may not use all the peripherals on the device. In that case, it may be desirable to disable unused peripherals. DEVDISR provides a mechanism for gating clocks to IP blocks that are not used when running an application. &lt;BR /&gt;You can enable/disable the TMU monitoring mode by configuring TMR[ME] mode bit. Please refer to chapter# 33 in the LS1046ARM for more details.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 06:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046-TMU-clock-config/m-p/1689041#M18518</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-07-20T06:45:02Z</dc:date>
    </item>
  </channel>
</rss>