<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX31: Flashing via ATK in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197011#M1844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have two IMX31ADS boards and one board of our own design that I cannot flash via ATK.&amp;nbsp; The HAB_TYPE displays as "Production".&amp;nbsp; I have one IMX31-3Stack board that I can flash via ATK.&amp;nbsp; In this case, HAB_TYPE is "Development/Disable".&amp;nbsp; Is the "Production" HAB_TYPE preventing me from flashing the uncooperative boards, and is there any way to change it?&lt;BR /&gt;&lt;BR /&gt;We have a Realview ICE at one of our locations, but we are doing IMX31 development across 3 different locations.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Oct 2008 01:36:16 GMT</pubDate>
    <dc:creator>Herg</dc:creator>
    <dc:date>2008-10-24T01:36:16Z</dc:date>
    <item>
      <title>IMX31: Flashing via ATK</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197011#M1844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have two IMX31ADS boards and one board of our own design that I cannot flash via ATK.&amp;nbsp; The HAB_TYPE displays as "Production".&amp;nbsp; I have one IMX31-3Stack board that I can flash via ATK.&amp;nbsp; In this case, HAB_TYPE is "Development/Disable".&amp;nbsp; Is the "Production" HAB_TYPE preventing me from flashing the uncooperative boards, and is there any way to change it?&lt;BR /&gt;&lt;BR /&gt;We have a Realview ICE at one of our locations, but we are doing IMX31 development across 3 different locations.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2008 01:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197011#M1844</guid>
      <dc:creator>Herg</dc:creator>
      <dc:date>2008-10-24T01:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: IMX31: Flashing via ATK</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197012#M1845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Looks like your MX31ADS are from an old revision. Can you check the silicon mask?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You need to burn a fuse to enable UART communication with ATK. Please follow the steps below:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;1. Turn off the ADS and remove the CPU board.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;2. Remove resistor R227 from the CPU board (it is located in the back of the board)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;3. Connect a jumper between 1-2 on JP37. (This puts FUSE_VDD&amp;nbsp;at 1.8 V)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;4. Insert the CPU board and turn on the ADS&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;5. Do a normal boot from NOR and get to Redboot prompt&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;6. Connect a jumper between&amp;nbsp;2-3 on JP37. ( This puts FUSE_VDD at 3.3V, which is required for blowing the fuses)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;7. Send the following command: "RedBoot&amp;gt; fuse_blow 0 5 1 "&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;8.&amp;nbsp;Confirm that the fuse was blown: "fuse_read 0 5" should read 0x1.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Arial" size="2"&gt;9. Connect a jumper between 1-2 on JP37&lt;/FONT&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2008 06:37:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197012#M1845</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2008-10-24T06:37:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX31: Flashing via ATK</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197013#M1846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The markings on the one I working with now:&lt;BR /&gt;PCIMX31VKN5&lt;BR /&gt;Q602ZYN.03 4&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0616&lt;BR /&gt;3L38W CHINA&lt;BR /&gt;&lt;BR /&gt;Following the instruction above, I was able to get it to work.&amp;nbsp; I did have to do "fuse_blow 0 5 0" before the "fuse_blow 0 5 1" would actually work.&amp;nbsp; If only I can figure out how to blow the fuse without needing Redboot already in NOR, I'll be in business.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Herg on &lt;SPAN class="date_text"&gt;2008-10-24&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;03:11 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2008 21:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197013#M1846</guid>
      <dc:creator>Herg</dc:creator>
      <dc:date>2008-10-24T21:09:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX31: Flashing via ATK</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197014#M1847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;You can use a JTAG debugger for loading the Redboot image directly into RAM. For the RealView tool you can find the initialization script inside the BSP iso. It is called init_ddr.inc.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Fabio Estevam&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2008 00:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IMX31-Flashing-via-ATK/m-p/197014#M1847</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2008-10-30T00:00:35Z</dc:date>
    </item>
  </channel>
</rss>