<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: MPC8548 with slave FPGA</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196864#M1841</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Hi&lt;BR /&gt;We have configured FPGA through GPO of MPC.&lt;BR /&gt;&lt;BR /&gt;Its just Slave Serial Interface needs to be done, it takes only few seconds.&lt;BR /&gt;&lt;BR /&gt;We need Register Level Programming details for TSEC.&lt;BR /&gt;&lt;BR /&gt;regards&lt;BR /&gt;ragh&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Nov 2008 21:19:23 GMT</pubDate>
    <dc:creator>IMX31</dc:creator>
    <dc:date>2008-11-24T21:19:23Z</dc:date>
    <item>
      <title>MPC8548 with slave FPGA</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196861#M1838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;As I have understood, the MPC8548 does not have any free general purpose IO (GPIO)? So in case I want that MCU uploads the configuration file to the FPGA via JTAG, how should I do it? Which pins of the MPC8548 I can use as a JTAG pins? Or should I connect some logic devices. like EPLD to the local bus and then there is a JTAG bus between EPLD and FPGA?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;&lt;BR /&gt;Karote&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2008 18:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196861#M1838</guid>
      <dc:creator>Karote</dc:creator>
      <dc:date>2008-02-27T18:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 with slave FPGA</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196862#M1839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Couldn't you load the FPGA through I2C? I've never seen someone do that by emulating JTAG.&lt;BR /&gt;&lt;BR /&gt;Anyway, there are GPIO available, depending on what features you're using. TSEC2 and PCI, for example, can be used either as their intended feature or as GPIO.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2008 21:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196862#M1839</guid>
      <dc:creator>genuap</dc:creator>
      <dc:date>2008-02-27T21:28:57Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 with slave FPGA</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196863#M1840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thank you for your answer.&lt;BR /&gt;&lt;BR /&gt;JTAG is more or less a debug interface in our case. Actually we want to connect the&amp;nbsp; MPC8548 with&amp;nbsp; Virtex5&amp;nbsp; FPGA using local bus. Does Freescale have any application note or&amp;nbsp; some white paper about&amp;nbsp; using local bus between FPGA and MCU? Mainly I'm interested which signals I have to route to the FPGA from the LBC?&lt;BR /&gt;&lt;BR /&gt;Another thing, is the FPGA considered as UPM device? (user programmable device)&lt;BR /&gt;&lt;BR /&gt;Local bus is enough for our purposes, so do not need any faster interface (I know that PCI and PCIxpress would be possible as well)&lt;BR /&gt;&lt;BR /&gt;Thank you in advance.&lt;BR /&gt;&lt;BR /&gt;Karote&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2008 19:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196863#M1840</guid>
      <dc:creator>Karote</dc:creator>
      <dc:date>2008-03-04T19:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 with slave FPGA</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196864#M1841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Hi&lt;BR /&gt;We have configured FPGA through GPO of MPC.&lt;BR /&gt;&lt;BR /&gt;Its just Slave Serial Interface needs to be done, it takes only few seconds.&lt;BR /&gt;&lt;BR /&gt;We need Register Level Programming details for TSEC.&lt;BR /&gt;&lt;BR /&gt;regards&lt;BR /&gt;ragh&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2008 21:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8548-with-slave-FPGA/m-p/196864#M1841</guid>
      <dc:creator>IMX31</dc:creator>
      <dc:date>2008-11-24T21:19:23Z</dc:date>
    </item>
  </channel>
</rss>