<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1027A PORESET in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683702#M18386</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am designing a CPU based on the LS1027A. In the reference manual LS1028ARM (Table 12) is defined the power-on sequence for that device. The question is related with the initial stages and PORESET.&lt;/P&gt;&lt;P&gt;Is it necessary to perform a full PORESET pulse (falling and rising edge) or is it enought to mantain PORESET low more than 1ms after all power rails are ok and then rise it to '1'?&lt;/P&gt;&lt;P&gt;If the second option is possible it is easy to do that with a voltage monitor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jul 2023 06:43:07 GMT</pubDate>
    <dc:creator>JOM_alor</dc:creator>
    <dc:date>2023-07-07T06:43:07Z</dc:date>
    <item>
      <title>LS1027A PORESET</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683702#M18386</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am designing a CPU based on the LS1027A. In the reference manual LS1028ARM (Table 12) is defined the power-on sequence for that device. The question is related with the initial stages and PORESET.&lt;/P&gt;&lt;P&gt;Is it necessary to perform a full PORESET pulse (falling and rising edge) or is it enought to mantain PORESET low more than 1ms after all power rails are ok and then rise it to '1'?&lt;/P&gt;&lt;P&gt;If the second option is possible it is easy to do that with a voltage monitor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 06:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683702#M18386</guid>
      <dc:creator>JOM_alor</dc:creator>
      <dc:date>2023-07-07T06:43:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A PORESET</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683855#M18397</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220037"&gt;@JOM_alor&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;The PORESET_B signal should be asserted for atleast 1ms after all the supply rails are stable.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 09:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683855#M18397</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-07-07T09:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A PORESET</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683863#M18398</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;OK. But the question is: should I assert PORESET_B with a "full" assertion pulse (1 ==&amp;gt; 0 ==&amp;gt; 1) or can I mantain PORESET_B al low level from power-supply startup and after at least 1ms deasset it (0 ==&amp;gt; 1)?&lt;/P&gt;&lt;P&gt;Many thanks for your fast answer!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jul 2023 09:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1683863#M18398</guid>
      <dc:creator>JOM_alor</dc:creator>
      <dc:date>2023-07-07T09:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A PORESET</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1684480#M18417</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220037"&gt;@JOM_alor&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;The PORESET_B signal must be low till the all the supplies are stable which means there will be 0==&amp;gt;1 logic.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 05:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1027A-PORESET/m-p/1684480#M18417</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-07-10T05:11:02Z</dc:date>
    </item>
  </channel>
</rss>