<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPI Macro in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SPI-Macro/m-p/1674204#M18242</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi, is it this macro &amp;lt;SPI_S_SPTEF_MASK&amp;gt; same function as &amp;lt;LPSPI_SR_TDF_MASK&amp;gt; ?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jun 2023 05:40:53 GMT</pubDate>
    <dc:creator>Jojo67</dc:creator>
    <dc:date>2023-06-22T05:40:53Z</dc:date>
    <item>
      <title>SPI Macro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SPI-Macro/m-p/1674204#M18242</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, is it this macro &amp;lt;SPI_S_SPTEF_MASK&amp;gt; same function as &amp;lt;LPSPI_SR_TDF_MASK&amp;gt; ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 05:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SPI-Macro/m-p/1674204#M18242</guid>
      <dc:creator>Jojo67</dc:creator>
      <dc:date>2023-06-22T05:40:53Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Macro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SPI-Macro/m-p/1674258#M18245</link>
      <description>&lt;P&gt;Hi SPI Macro can be defined following two types,&lt;/P&gt;&lt;P&gt;SPI_S_SPTEF_MASK&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is a mask for the SPI Transmit Buffer Empty Flag (SPTEF) in the SPI Status Register (SPI_S).&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the other hand,&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;LPSPI_SR_TDF_MASK&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is a mask for the Transmit Data Flag (TDF) in the LPSPI Status Register (LPSPI_SR).&lt;/P&gt;&lt;P&gt;Both of these masks are used to check the status of the respective SPI modules' transmit buffers, but they are specific to different SPI modules within the NXP product range. The&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;SPI_S_SPTEF_MASK&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is used with the classic SPI module, while the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;LPSPI_SR_TDF_MASK&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;is used with the Low Power SPI (LPSPI) module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information on these modules and their respective registers, you can refer to the following documentation:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers-Knowledge/SPI-Module-Registers-Configuration-Examples/ta-p/1115479" target="_blank" rel="noopener"&gt;SPI Module Registers Configuration Examples&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers-Knowledge/LPSPI-Module-Registers-Configuration-Examples/ta-p/1115480" target="_blank" rel="noopener"&gt;LPSPI Module Registers Configuration Examples&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Let me know if you need anymore help.&lt;BR /&gt;Kind Regards,&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 22 Jun 2023 07:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SPI-Macro/m-p/1674258#M18245</guid>
      <dc:creator>giraffe508</dc:creator>
      <dc:date>2023-06-22T07:34:59Z</dc:date>
    </item>
  </channel>
</rss>