<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: MC10XS4200 current level</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1668655#M18141</link>
    <description>Tomas, thanks a lot for your speedy response</description>
    <pubDate>Tue, 13 Jun 2023 22:08:27 GMT</pubDate>
    <dc:creator>mertsahin</dc:creator>
    <dc:date>2023-06-13T22:08:27Z</dc:date>
    <item>
      <title>MC10XS4200 current level</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1667950#M18121</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to drive 27 V motor which has continuous current 6 A and instantaneous current 30 A for 2 seconds.&lt;/P&gt;&lt;P&gt;1) Can this part handle it? If not should I use 6 mohm version?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) Is it possible to parallel multipke&amp;nbsp;&lt;SPAN&gt;MC10XS4200 devices to obtain more current?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3) If not 2 seconds possible then how many ms can this device withstand to 30 A ins. current?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks a lot.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 05:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1667950#M18121</guid>
      <dc:creator>mertsahin</dc:creator>
      <dc:date>2023-06-13T05:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: MC10XS4200 current level</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1668084#M18131</link>
      <description>&lt;P&gt;Hi Mert,&lt;/P&gt;
&lt;P&gt;The MC10XS4200 cannot drive 30A for 2 seconds, you can find the timing as below.&lt;/P&gt;
&lt;P&gt;The max. timing is 350ms when motor current goes up. Even in parallel, current can be doubled, but time is fixed.&lt;/P&gt;
&lt;P&gt;You can use the MC06XS4200 due to DC current up to 15A, use two outputs in parallel, then current is also doubled to 30A.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 614px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227334iEC14F1688242E8EF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture 1.JPG" style="width: 720px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227335i1F287B52A3D49F71/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture 1.JPG" alt="Capture 1.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture 1.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 07:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1668084#M18131</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-06-13T07:38:16Z</dc:date>
    </item>
    <item>
      <title>Re: MC10XS4200 current level</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1668655#M18141</link>
      <description>Tomas, thanks a lot for your speedy response</description>
      <pubDate>Tue, 13 Jun 2023 22:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC10XS4200-current-level/m-p/1668655#M18141</guid>
      <dc:creator>mertsahin</dc:creator>
      <dc:date>2023-06-13T22:08:27Z</dc:date>
    </item>
  </channel>
</rss>