<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: iMX21 USB device linux driver</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190905#M1738</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But is not possible to take 2.6.30 kernel from the kernel archive and try to compile it using ltib,.. I see two options in ltib if we select for local linux directory build ie., to enter the linux source directory and kbuild_output path(??),.. did you also select the same thing and compile hte microcross kernel. and ofcourse lot of patches will be required to be put to the kernel ofcourse&lt;/P&gt;&lt;P&gt;well, thanks for the imm reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2009 19:13:45 GMT</pubDate>
    <dc:creator>Kewal</dc:creator>
    <dc:date>2009-06-24T19:13:45Z</dc:date>
    <item>
      <title>iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190902#M1735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to use the OTG port as device (function) under linux 2.6.11. On the net I found a imx_udc.c driver by Mike Lee but it is for iMX1. The porting is not trivial because the controllers are very different.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there anyone who found something for iMX21?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2009 20:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190902#M1735</guid>
      <dc:creator>Denis3</dc:creator>
      <dc:date>2009-06-17T20:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190903#M1736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I dont have a solution for your question rather I am also trying to find a driver to get the OTG working on imx21ads. However, I wanted to ask which tools you are using (LTIB, crosscompilers)to get the 2.6 kernel on to the board. Currently I am using 2.4.20 on my board which I want to upgrade it to 2.6.30 or any 2.6 kernel. wanted some hints regarding 2.6 kernel on imx21 .&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2009 13:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190903#M1736</guid>
      <dc:creator>Kewal</dc:creator>
      <dc:date>2009-06-24T13:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190904#M1737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we used kernel 2.6.11 from Microcross. You can find the LTIB &lt;A href="http://www.bitshrine.org/" rel="nofollow" target="_blank"&gt;here&lt;/A&gt;. As crosscompiler you can download the crosstools from &lt;A href="http://www.kegel.com/crosstool/" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; and the build your own ARM toolchain.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope it helped.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2009 14:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190904#M1737</guid>
      <dc:creator>Denis3</dc:creator>
      <dc:date>2009-06-24T14:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190905#M1738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But is not possible to take 2.6.30 kernel from the kernel archive and try to compile it using ltib,.. I see two options in ltib if we select for local linux directory build ie., to enter the linux source directory and kbuild_output path(??),.. did you also select the same thing and compile hte microcross kernel. and ofcourse lot of patches will be required to be put to the kernel ofcourse&lt;/P&gt;&lt;P&gt;well, thanks for the imm reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2009 19:13:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190905#M1738</guid>
      <dc:creator>Kewal</dc:creator>
      <dc:date>2009-06-24T19:13:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190906#M1739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used ltib only to build a jffs2 filesystem. I compile the kernel on his own.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Obviously you can't take the kernel from kernel.org and make it run on your board out of the box. You need to make a port and this is not an easy task. If you don't need specific features that are present only on 2.6.30 I suggest you to take from microcross the latest version ported to imx21. Probably you'll have to make some modification to make it run on your board but al least it's a good start point.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2009 17:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190906#M1739</guid>
      <dc:creator>Denis3</dc:creator>
      <dc:date>2009-06-25T17:28:43Z</dc:date>
    </item>
    <item>
      <title>Re: iMX21 USB device linux driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190907#M1740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MX21ADS is supported in mainline kernel:&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.kernel.org/?p=linux/kernel/git/torvalds/linux-2.6.git;a=tree;f=arch/arm/mach-mx2;h=63d185da97fbdc2c9f3d58daeadb63b1612cda6c;hb=master" rel="nofollow" target="_blank"&gt;http://git.kernel.org/?p=linux/kernel/git/torvalds/linux-2.6.git;a=tree;f=arch/arm/mach-mx2;h=63d185da97fbdc2c9f3d58daeadb63b1612cda6c;hb=master&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2009 09:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/iMX21-USB-device-linux-driver/m-p/190907#M1740</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2009-06-26T09:12:22Z</dc:date>
    </item>
  </channel>
</rss>