<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JN5189 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1622039#M17186</link>
    <description>&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;My SDK version is 2.6.5(2022-3-10).&lt;/P&gt;&lt;P&gt;I modify the data in g_buffer(/* Set the buffer */&lt;BR /&gt;for (i = 0; i &amp;lt; PAGE_SIZE; i++)&lt;BR /&gt;{&lt;BR /&gt;g_buffer[i] = i;&lt;BR /&gt;}),&amp;nbsp;&lt;/P&gt;&lt;P&gt;print the data in the flash(val = (uint8_t *)(FSL_FEATURE_SPIFI_START_ADDR + i);&lt;BR /&gt;PRINTF(" %d %d ", i, *val);) ,&lt;/P&gt;&lt;P&gt;download the program to the target board and open the serial terminal,the data read print is different from the data written.&lt;/P&gt;&lt;P&gt;So,i restore the original program,it also can not print the data .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 26 Mar 2023 07:15:05 GMT</pubDate>
    <dc:creator>paidaxing</dc:creator>
    <dc:date>2023-03-26T07:15:05Z</dc:date>
    <item>
      <title>JN5189</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1621448#M17171</link>
      <description>Hello, my question:When i use the jn5189dk6_spi_polling_transfer in SDK example,i change the data I change the written data, it can't read out stably.</description>
      <pubDate>Fri, 24 Mar 2023 07:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1621448#M17171</guid>
      <dc:creator>paidaxing</dc:creator>
      <dc:date>2023-03-24T07:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1621921#M17183</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214162"&gt;@paidaxing&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Just to confirm, which version of the SDK are you using?&lt;BR /&gt;&lt;BR /&gt;Could you please clarify what do you mean with "can't read out stably"? Does the example without modifications work properly? Is it possible for you to capture the data transmission with a logic analyzer/oscilloscope?&lt;BR /&gt;&lt;BR /&gt;Could you please help us with more details about the main modifications you have done to the base project? How are you modifying the source buffer?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 23:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1621921#M17183</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-03-24T23:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1622039#M17186</link>
      <description>&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;My SDK version is 2.6.5(2022-3-10).&lt;/P&gt;&lt;P&gt;I modify the data in g_buffer(/* Set the buffer */&lt;BR /&gt;for (i = 0; i &amp;lt; PAGE_SIZE; i++)&lt;BR /&gt;{&lt;BR /&gt;g_buffer[i] = i;&lt;BR /&gt;}),&amp;nbsp;&lt;/P&gt;&lt;P&gt;print the data in the flash(val = (uint8_t *)(FSL_FEATURE_SPIFI_START_ADDR + i);&lt;BR /&gt;PRINTF(" %d %d ", i, *val);) ,&lt;/P&gt;&lt;P&gt;download the program to the target board and open the serial terminal,the data read print is different from the data written.&lt;/P&gt;&lt;P&gt;So,i restore the original program,it also can not print the data .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 26 Mar 2023 07:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1622039#M17186</guid>
      <dc:creator>paidaxing</dc:creator>
      <dc:date>2023-03-26T07:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1622044#M17187</link>
      <description>Thank you for you replay,I change the SDK ,the problem has resloved.</description>
      <pubDate>Sun, 26 Mar 2023 08:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/JN5189/m-p/1622044#M17187</guid>
      <dc:creator>paidaxing</dc:creator>
      <dc:date>2023-03-26T08:35:35Z</dc:date>
    </item>
  </channel>
</rss>