<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックCan't access PCIe in s32v234 boards</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1621819#M17182</link>
    <description>&lt;P&gt;Tried to access the PCIe device on two s32v234 boards, unsuccessfully.&lt;/P&gt;&lt;P&gt;In U-Boot, pci commands, such as enum, get a "pci_bus_to_hose() failed" message.&lt;/P&gt;&lt;P&gt;With Lauterbach, tried accessing the PCIe section in its built-in register mechanism, and also accessing directly the address stated in the Reference Manual (0x72000000 - 0x72ffffff). In both cases I get a debug port time out error.&lt;/P&gt;&lt;P&gt;Does U-Boot not clock the PCIe bus on this board? Is it disabled through some other means?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Mar 2023 16:20:04 GMT</pubDate>
    <dc:creator>steven_leon</dc:creator>
    <dc:date>2023-03-24T16:20:04Z</dc:date>
    <item>
      <title>Can't access PCIe in s32v234 boards</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1621819#M17182</link>
      <description>&lt;P&gt;Tried to access the PCIe device on two s32v234 boards, unsuccessfully.&lt;/P&gt;&lt;P&gt;In U-Boot, pci commands, such as enum, get a "pci_bus_to_hose() failed" message.&lt;/P&gt;&lt;P&gt;With Lauterbach, tried accessing the PCIe section in its built-in register mechanism, and also accessing directly the address stated in the Reference Manual (0x72000000 - 0x72ffffff). In both cases I get a debug port time out error.&lt;/P&gt;&lt;P&gt;Does U-Boot not clock the PCIe bus on this board? Is it disabled through some other means?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 16:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1621819#M17182</guid>
      <dc:creator>steven_leon</dc:creator>
      <dc:date>2023-03-24T16:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: Can't access PCIe in s32v234 boards</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1625290#M17255</link>
      <description>&lt;P&gt;Hi Stevon&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you have raised new ticket in nxp as "&lt;SPAN&gt;PCIe inaccessible in s32v234 boards" . this both ticket are same. can we close here and continue in nxp support ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards ,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Tushar&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 12:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1625290#M17255</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-03-30T12:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: Can't access PCIe in s32v234 boards</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1625535#M17258</link>
      <description>&lt;P&gt;Hi Tushar,&lt;/P&gt;&lt;P&gt;That's correct, same topic.&lt;/P&gt;&lt;P&gt;Yes, it can be closed here.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 19:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Can-t-access-PCIe-in-s32v234-boards/m-p/1625535#M17258</guid>
      <dc:creator>steven_leon</dc:creator>
      <dc:date>2023-03-30T19:12:07Z</dc:date>
    </item>
  </channel>
</rss>