<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックWhat is the address of the MPC8313E-RDB LED/Status buffer (LCS3)?</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/What-is-the-address-of-the-MPC8313E-RDB-LED-Status-buffer-LCS3/m-p/190215#M1705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Fellow Freescale MPC8313E users,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've been looking through all the manuals/docs I can find from Freescale, but have been unable to find one thing I need for my project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running the latest Linux BSP for the MPC8313E-RDB board and need to manipulate the onboard LEDs (either write&amp;nbsp;the C code&amp;nbsp;myself, or use a library if one is available). What I can't find is the actual physical address to write out to set/clear the onborad debug LEDs. According to the user guide it is mapped to LCS3 on the chip, but I can't find anything to say what address is mapped to LCS3. I assume the BSP or UBOOT load is setting a map between LCS3 and an actual physical address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone post the actual address for writing to the LEDs (should be same address as reading from the status buffer) or if there it is in a Freescale document please point me to that document?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;abartky&lt;/P&gt;&lt;FONT face="Arial" size="2"&gt;&lt;/FONT&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 16 Feb 2008 03:29:40 GMT</pubDate>
    <dc:creator>abartky</dc:creator>
    <dc:date>2008-02-16T03:29:40Z</dc:date>
    <item>
      <title>What is the address of the MPC8313E-RDB LED/Status buffer (LCS3)?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/What-is-the-address-of-the-MPC8313E-RDB-LED-Status-buffer-LCS3/m-p/190215#M1705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Fellow Freescale MPC8313E users,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've been looking through all the manuals/docs I can find from Freescale, but have been unable to find one thing I need for my project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running the latest Linux BSP for the MPC8313E-RDB board and need to manipulate the onboard LEDs (either write&amp;nbsp;the C code&amp;nbsp;myself, or use a library if one is available). What I can't find is the actual physical address to write out to set/clear the onborad debug LEDs. According to the user guide it is mapped to LCS3 on the chip, but I can't find anything to say what address is mapped to LCS3. I assume the BSP or UBOOT load is setting a map between LCS3 and an actual physical address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone post the actual address for writing to the LEDs (should be same address as reading from the status buffer) or if there it is in a Freescale document please point me to that document?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;abartky&lt;/P&gt;&lt;FONT face="Arial" size="2"&gt;&lt;/FONT&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2008 03:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/What-is-the-address-of-the-MPC8313E-RDB-LED-Status-buffer-LCS3/m-p/190215#M1705</guid>
      <dc:creator>abartky</dc:creator>
      <dc:date>2008-02-16T03:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: What is the address of the MPC8313E-RDB LED/Status buffer (LCS3)?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/What-is-the-address-of-the-MPC8313E-RDB-LED-Status-buffer-LCS3/m-p/190216#M1706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After doing some more hunting I found the info I needed, I am posting this message in case someone else has the same problem I had&amp;nbsp;finding the info.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to find a good memory map on the MPC8313E-RDB Board Support Package and Documentaiton CDROM that came with the board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The file: /help/hardware/8313evb_init.cfg has a full memory map. The MPC8313E-RDB LED/Status buffer is at 0xFA000000 and I have verified that with a small C command line utility I wrote and I also have it running in my IEEE 1588 / IEEE 802.1AS Precision Time Protocol stack. Here is an excerpt from that file with other addresses that may be of interest/use:&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;##############################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# System Configuration - Local Access Windows&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;##############################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# Local Bus Local Access Windows&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;#################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 0 - FLASH&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000020 0xfe000000 # LBLAWBAR0 - begining at 0xff000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000024 0x80000017 # LBLAWAR0 - enable, size = 16MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 1 - NAND Flash&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000028 0xf8000000 # LBLAWBAR1 - begining at 0xf8000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe000002c 0x80000018 # LBLAWAR1 - enable, size = 32MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 2 - VSC7385&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000030 0xf0000000 # LBLAWBAR2 - begining at 0xfc100000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000034 0x80000010 # LBLAWAR2 - enable, size = 128kB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 3 - Read Write Buffer&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000038 0xfa000000 # LBLAWBAR3 - begining at 0xfa000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe000003c 0x8000000e # LBLAWAR3 - enable, size = 32kB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# PCI Local Access Windows&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;#################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 0&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000060 0x80000000 # PCILAWBAR0 - begining at 0x80000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000064 0x8000001c # PCILAWAR0 - enable, size = 512MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 1&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe0000068 0xa0000000 # PCILAWBAR1 - begining at 0xa0000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe000006c 0x8000001c # PCILAWAR1 - enable, size = 512MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# DDR Local Access Windows&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;#################################&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 0 - 1st DDR SODIMM&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe00000a0 0x00000000 # DDRLAWBAR0 - begining at 0x00000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe00000a4 0x8000001a # DDRLAWAR0 - enable, size = 128MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;# WINDOW 1 - 2nd DDR SODIMM&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;#writemem.l 0xe00000a8 0x10000000 # DDRLAWBAR1 - begining at 0x10000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;#writemem.l 0xe00000ac 0x8000001b # DDRLAWAR1 - enable, size = 256MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe00000e0 0x08000000 # DDRLAWBAR0 - begining at 0x08000000&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;writemem.l 0xe00000e4 0x8000001a # DDRLAWAR0 - enable, size = 128MB&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;- abartky&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Feb 2008 05:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/What-is-the-address-of-the-MPC8313E-RDB-LED-Status-buffer-LCS3/m-p/190216#M1706</guid>
      <dc:creator>abartky</dc:creator>
      <dc:date>2008-02-17T05:51:52Z</dc:date>
    </item>
  </channel>
</rss>