<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: AR6000 Self-Start &amp;amp; LIN LDF support</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611750#M16958</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply.&lt;BR /&gt;&lt;BR /&gt;The unit I am working with is from Valeo 443546, after searching some technical documents I was able to identify the 4 pins used by the OEM.&lt;BR /&gt;&lt;BR /&gt;I am attempting to activate the motor function of the Alternator. I can look for more identification numbers if needed or if you can point me in the location where to locate them. It would be beneficial if I could find the right block that is being used.&lt;BR /&gt;&lt;BR /&gt;Reading the AR6000&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;See image,&lt;BR /&gt;&lt;BR /&gt;(Atleast pin out according to OEM configuration)&lt;BR /&gt;&lt;BR /&gt;Pin 1 is Ground (Pin 3 on AR6000)&lt;BR /&gt;Pin 2 is LIN&amp;nbsp;(Pin 4 on AR6000)&lt;BR /&gt;Pin 4 is Signal&amp;nbsp;(Pin 5? on AR6000)&lt;BR /&gt;Pin 5 is 12v (Pin 2 on AR6000)&lt;BR /&gt;Pin 3 is not used (Pin 1? on AR6000, assuming this is no manually control voltage instead of LIN to override Default voltage?)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Roll92_0-1678290148572.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213764i5100379B28527D15/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Roll92_0-1678290148572.png" alt="Roll92_0-1678290148572.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do see that Valeo&amp;nbsp;&lt;SPAN&gt;439866 has just inhibit crank and crank pin but I believe this is on the&amp;nbsp;TC80310&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Roll92_0-1678291392204.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213765i35377AC3B0998606/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Roll92_0-1678291392204.png" alt="Roll92_0-1678291392204.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Mar 2023 16:06:45 GMT</pubDate>
    <dc:creator>Roll92</dc:creator>
    <dc:date>2023-03-08T16:06:45Z</dc:date>
    <item>
      <title>AR6000 Self-Start &amp; LIN LDF support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611577#M16956</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am a hobbyist&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;enthusiast and am using a product that contains the AR6000 (Atleast it should)&lt;BR /&gt;&lt;BR /&gt;Looking at the Datasheet file it states that it does not use LIN for the Start/Stop capability and even with out LIN it will use the default values.&lt;BR /&gt;&lt;BR /&gt;Now as I see it, as a assembled product OEM's are only using 4 pin to operate the Alternator.&lt;BR /&gt;1 pin for 12v power, 1 pin for ground, 1 pin for LIN, and 1 pin for signal.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;From reading the datasheet file the pin for signal should be the one that triggers the Alternator to spin to either 3000rpm or 4000rpm.&lt;BR /&gt;&lt;BR /&gt;What type of signal is it? Ground signal? 0-5v signal? PWM? If PWM at what frequency?&lt;BR /&gt;&lt;BR /&gt;If anybody has a LDF file avaible for the LIN that would be much appreciate as it would save me alot of time.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 10:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611577#M16956</guid>
      <dc:creator>Roll92</dc:creator>
      <dc:date>2023-03-08T10:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: AR6000 Self-Start &amp; LIN LDF support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611632#M16957</link>
      <description>&lt;P&gt;Hello Andres,&lt;/P&gt;
&lt;P&gt;Could you share more details on the product you are using and what pin of the AR6000 you are referring to?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 3.JPG" style="width: 669px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213728i8CBAD5FEBCD101D6/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 3.JPG" alt="Table 3.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.JPG" style="width: 676px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213729iB496126A400DBEB7/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.JPG" alt="Capture.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 12:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611632#M16957</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-03-08T12:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: AR6000 Self-Start &amp; LIN LDF support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611750#M16958</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for the reply.&lt;BR /&gt;&lt;BR /&gt;The unit I am working with is from Valeo 443546, after searching some technical documents I was able to identify the 4 pins used by the OEM.&lt;BR /&gt;&lt;BR /&gt;I am attempting to activate the motor function of the Alternator. I can look for more identification numbers if needed or if you can point me in the location where to locate them. It would be beneficial if I could find the right block that is being used.&lt;BR /&gt;&lt;BR /&gt;Reading the AR6000&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;See image,&lt;BR /&gt;&lt;BR /&gt;(Atleast pin out according to OEM configuration)&lt;BR /&gt;&lt;BR /&gt;Pin 1 is Ground (Pin 3 on AR6000)&lt;BR /&gt;Pin 2 is LIN&amp;nbsp;(Pin 4 on AR6000)&lt;BR /&gt;Pin 4 is Signal&amp;nbsp;(Pin 5? on AR6000)&lt;BR /&gt;Pin 5 is 12v (Pin 2 on AR6000)&lt;BR /&gt;Pin 3 is not used (Pin 1? on AR6000, assuming this is no manually control voltage instead of LIN to override Default voltage?)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Roll92_0-1678290148572.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213764i5100379B28527D15/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Roll92_0-1678290148572.png" alt="Roll92_0-1678290148572.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do see that Valeo&amp;nbsp;&lt;SPAN&gt;439866 has just inhibit crank and crank pin but I believe this is on the&amp;nbsp;TC80310&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Roll92_0-1678291392204.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/213765i35377AC3B0998606/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Roll92_0-1678291392204.png" alt="Roll92_0-1678291392204.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Mar 2023 16:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1611750#M16958</guid>
      <dc:creator>Roll92</dc:creator>
      <dc:date>2023-03-08T16:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: AR6000 Self-Start &amp; LIN LDF support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1614168#M17015</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12216"&gt;@TomasVaverka&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Do you know what the trigger is for the start stop function is? Is it a analog signal or pwm?&lt;BR /&gt;&lt;BR /&gt;LDF files available?&lt;BR /&gt;&lt;BR /&gt;Best regards &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 14:57:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1614168#M17015</guid>
      <dc:creator>Roll92</dc:creator>
      <dc:date>2023-03-13T14:57:14Z</dc:date>
    </item>
    <item>
      <title>Re: AR6000 Self-Start &amp; LIN LDF support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1660507#M17943</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/12216"&gt;@TomasVaverka&lt;/a&gt;&amp;nbsp;Do you know what signal the PH needs to see to initiate Self start? What frequency?&lt;/P&gt;</description>
      <pubDate>Wed, 31 May 2023 07:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/AR6000-Self-Start-amp-LIN-LDF-support/m-p/1660507#M17943</guid>
      <dc:creator>Roll92</dc:creator>
      <dc:date>2023-05-31T07:07:29Z</dc:date>
    </item>
  </channel>
</rss>