<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IEC 60730 Library in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IEC-60730-Library/m-p/1586345#M16491</link>
    <description>&lt;P&gt;I have a few questions about the test library implementation.&lt;/P&gt;&lt;P&gt;For the data pinDir value in the digital IO setting what should the value for this be?&amp;nbsp; My assumption is that it would be 0 for input and 1 for output.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;For the pinMux I am not sure what to put in this value.&amp;nbsp; I am not multiplexing this pin so my assumption is that the value would be 0.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;For the clock and watch dog tests what are the values for the limits?&amp;nbsp; Are they just the clock ticks?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 21 Jan 2023 15:06:04 GMT</pubDate>
    <dc:creator>pbaierlac</dc:creator>
    <dc:date>2023-01-21T15:06:04Z</dc:date>
    <item>
      <title>IEC 60730 Library</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IEC-60730-Library/m-p/1586345#M16491</link>
      <description>&lt;P&gt;I have a few questions about the test library implementation.&lt;/P&gt;&lt;P&gt;For the data pinDir value in the digital IO setting what should the value for this be?&amp;nbsp; My assumption is that it would be 0 for input and 1 for output.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;For the pinMux I am not sure what to put in this value.&amp;nbsp; I am not multiplexing this pin so my assumption is that the value would be 0.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;For the clock and watch dog tests what are the values for the limits?&amp;nbsp; Are they just the clock ticks?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 21 Jan 2023 15:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IEC-60730-Library/m-p/1586345#M16491</guid>
      <dc:creator>pbaierlac</dc:creator>
      <dc:date>2023-01-21T15:06:04Z</dc:date>
    </item>
  </channel>
</rss>