<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K32L2B3 using keil uvision in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1570270#M16107</link>
    <description>Thanks Carlos&lt;BR /&gt;Another question if you can help me.&lt;BR /&gt;If I program the microcontroller located on the board through JTAG it is not necessary to import the libreries dedicated to the board in order to have a working project. Correct? This is because I want to use only the micro to develop a clean FW that will then be destined for a proprietary device that we are developing of which I do not yet possess the finished PCB. Obviously it will be my responsibility to manage the offered periphery from the board like led Input/output pin if it is necessary.&lt;BR /&gt;Thanks</description>
    <pubDate>Thu, 15 Dec 2022 08:13:48 GMT</pubDate>
    <dc:creator>Saimon</dc:creator>
    <dc:date>2022-12-15T08:13:48Z</dc:date>
    <item>
      <title>FRDM-K32L2B3 using keil uvision</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1568910#M16098</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Hello&lt;BR /&gt;I want to develop a project on MCU K32L2B31VLH0A.&lt;BR /&gt;I want to use de development board FRDM-K32L2B3 and trasfer this project with JTAG using ULINK2.&lt;BR /&gt;I need help to set up the uvison KEIL ambient for realized a simple program like blinking a led and transfer it to the board to ensure tha all it work.&lt;BR /&gt;Is there somebody that can say me what kind of software component i need to choose in minimal configuration for this task?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="a.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/204204i4FAE0AF4FF6F6097/image-size/medium?v=v2&amp;amp;px=400" role="button" title="a.png" alt="a.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Tue, 13 Dec 2022 09:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1568910#M16098</guid>
      <dc:creator>Saimon</dc:creator>
      <dc:date>2022-12-13T09:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K32L2B3 using keil uvision</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1569287#M16102</link>
      <description>&lt;P style="margin: 0in; font-family: Montserrat; font-size: 12.0pt;" lang="es-MX"&gt;This tutorial can help you with the start coding with that board&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Montserrat; font-size: 12.0pt;" lang="es-MX"&gt;&lt;A href="https://developer.arm.com/documentation/kan299/latest/" target="_blank"&gt;https://developer.arm.com/documentation/kan299/latest/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Dec 2022 02:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1569287#M16102</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-12-14T02:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K32L2B3 using keil uvision</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1570270#M16107</link>
      <description>Thanks Carlos&lt;BR /&gt;Another question if you can help me.&lt;BR /&gt;If I program the microcontroller located on the board through JTAG it is not necessary to import the libreries dedicated to the board in order to have a working project. Correct? This is because I want to use only the micro to develop a clean FW that will then be destined for a proprietary device that we are developing of which I do not yet possess the finished PCB. Obviously it will be my responsibility to manage the offered periphery from the board like led Input/output pin if it is necessary.&lt;BR /&gt;Thanks</description>
      <pubDate>Thu, 15 Dec 2022 08:13:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1570270#M16107</guid>
      <dc:creator>Saimon</dc:creator>
      <dc:date>2022-12-15T08:13:48Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K32L2B3 using keil uvision</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1573219#M16140</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/209965"&gt;@Saimon&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;It should not be necessary to import the libraries in order to program through JTAG.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Just take care of the pin muxing that you will use for JTAG, remember not to use them for other functionality.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Regards, Raul.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 16:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FRDM-K32L2B3-using-keil-uvision/m-p/1573219#M16140</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2022-12-21T16:19:01Z</dc:date>
    </item>
  </channel>
</rss>