<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Ethernet boot boot-patch</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-boot-boot-patch/m-p/187576#M1563</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;I generated a boot patch for DDR for the EVM. Provided the patch in your other thread regarding ethernet boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flow is this:&lt;/P&gt;&lt;P&gt;1. Burn the boot patch file to the board's I2C EEPROM using the standard I2C Burner project in the CodeWarrior directory base&lt;/P&gt;&lt;P&gt;(Freescale\CW SC v10.2.x\SC\StarCore_Support\I2CBoot\MSC815x-MSC825x\EEPROM_burner)&lt;/P&gt;&lt;P&gt;2. Change dip switches or your RCW settings so that BP == 1. (If you are configuring RCW from the I2C Rom, that means you have to update the boot patch file with your desired settings there, including BP).&lt;/P&gt;&lt;P&gt;3. Repower the board and boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then the board will start the boot process, pause boot and run the boot patch (in the case of the patch I sent - it will set up the DDR Controller for the EVM), and then it will return to the standard Boot process.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Dec 2011 05:05:32 GMT</pubDate>
    <dc:creator>AndrewinApps</dc:creator>
    <dc:date>2011-12-17T05:05:32Z</dc:date>
    <item>
      <title>Ethernet boot boot-patch</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-boot-boot-patch/m-p/187575#M1562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before I lunge in at the deep end trying to flash EEPROM's, does anyone have any hints / tips / suggestions / comments / step-by-step guides on using the boot-patch for boot-over-ethernet configurations on a MSC8156EVM board?I find the documentation on it oddly cryptic and in some places confusing...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help gratefully received.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2011 19:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-boot-boot-patch/m-p/187575#M1562</guid>
      <dc:creator>TimeLord86</dc:creator>
      <dc:date>2011-12-02T19:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet boot boot-patch</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-boot-boot-patch/m-p/187576#M1563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;I generated a boot patch for DDR for the EVM. Provided the patch in your other thread regarding ethernet boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The flow is this:&lt;/P&gt;&lt;P&gt;1. Burn the boot patch file to the board's I2C EEPROM using the standard I2C Burner project in the CodeWarrior directory base&lt;/P&gt;&lt;P&gt;(Freescale\CW SC v10.2.x\SC\StarCore_Support\I2CBoot\MSC815x-MSC825x\EEPROM_burner)&lt;/P&gt;&lt;P&gt;2. Change dip switches or your RCW settings so that BP == 1. (If you are configuring RCW from the I2C Rom, that means you have to update the boot patch file with your desired settings there, including BP).&lt;/P&gt;&lt;P&gt;3. Repower the board and boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then the board will start the boot process, pause boot and run the boot patch (in the case of the patch I sent - it will set up the DDR Controller for the EVM), and then it will return to the standard Boot process.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Dec 2011 05:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-boot-boot-patch/m-p/187576#M1563</guid>
      <dc:creator>AndrewinApps</dc:creator>
      <dc:date>2011-12-17T05:05:32Z</dc:date>
    </item>
  </channel>
</rss>