<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Creating files in root file system in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187496#M1557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;I have a question regarding file system produced by BSP for MPC8308 evaluation board.&lt;BR /&gt;&lt;BR /&gt;I start Linux with "run flashramboot" command in U-Boot. Then in Linux I can successfully create some files in file system. But after restart all files disappear. I tried to create files in different folders: "/", "/home/user", may be somewhere else... and everywhere they disappear after reboot.&lt;BR /&gt;&lt;BR /&gt;I checked in LTIB configuration that "read-only filesystem" option is not enabled... So at the moment I don't understand such behavior...&lt;BR /&gt;&lt;BR /&gt;File system type is ext2.gz&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does somebody have some explanation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Aug 2012 15:00:55 GMT</pubDate>
    <dc:creator>Nich</dc:creator>
    <dc:date>2012-08-09T15:00:55Z</dc:date>
    <item>
      <title>Creating files in root file system</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187496#M1557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;I have a question regarding file system produced by BSP for MPC8308 evaluation board.&lt;BR /&gt;&lt;BR /&gt;I start Linux with "run flashramboot" command in U-Boot. Then in Linux I can successfully create some files in file system. But after restart all files disappear. I tried to create files in different folders: "/", "/home/user", may be somewhere else... and everywhere they disappear after reboot.&lt;BR /&gt;&lt;BR /&gt;I checked in LTIB configuration that "read-only filesystem" option is not enabled... So at the moment I don't understand such behavior...&lt;BR /&gt;&lt;BR /&gt;File system type is ext2.gz&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does somebody have some explanation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Aug 2012 15:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187496#M1557</guid>
      <dc:creator>Nich</dc:creator>
      <dc:date>2012-08-09T15:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: Creating files in root file system</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187497#M1558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Google for "ext.gz". ".gz" usually means "compressed with gzip". I'd say it is certainly a compressed read-only file system.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Type "mount" and see if there are any other partitions mounted that aren't compressed. Otherwise you'll need to add some.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe you're meant to plug in an SD card or a USB Memory stick and use that as the read-write file system?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2012 08:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187497#M1558</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2012-08-10T08:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: Creating files in root file system</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187498#M1559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have already realized that. Thanks for your response anyway.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2012 13:48:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Creating-files-in-root-file-system/m-p/187498#M1559</guid>
      <dc:creator>Nich</dc:creator>
      <dc:date>2012-08-10T13:48:05Z</dc:date>
    </item>
  </channel>
</rss>