<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Config SJA1105ELY</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Config-SJA1105ELY/m-p/1533344#M15442</link>
    <description>&lt;P&gt;Hi Lukas,&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you tell me what HW are you using exactly?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And also - assuming you are using the python tools to generate the configuration - can you provide the script you used?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;</description>
    <pubDate>Thu, 06 Oct 2022 11:13:17 GMT</pubDate>
    <dc:creator>kaden</dc:creator>
    <dc:date>2022-10-06T11:13:17Z</dc:date>
    <item>
      <title>Config SJA1105ELY</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Config-SJA1105ELY/m-p/1530451#M15400</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;i have problems with the config of the&amp;nbsp;SJA1105ELY switch. i created a config with the gen tool, but my conif isn't valid--&amp;gt;the configs-bit=0.&lt;/P&gt;&lt;P&gt;I'm not sure if my HW ist the problem, or my SPI-Bus. i can read the device id (address 0x00) and also the bits 3:0 from the configuration status information--&amp;gt;counter changes.&lt;/P&gt;&lt;P&gt;However i can't read any reset-values like&amp;nbsp; 12121212h from address&amp;nbsp;100800h.&lt;/P&gt;&lt;P&gt;Also the MISO line isn't responding the way i think it should. It only mirrors the address that i send via MOSI line&lt;/P&gt;&lt;P&gt;Anyone has an idea what the problem ist?&lt;/P&gt;&lt;P&gt;btw i try to config the&amp;nbsp;SJA1105ELY with an ESP32&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Yours Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 12:48:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Config-SJA1105ELY/m-p/1530451#M15400</guid>
      <dc:creator>Lukas4</dc:creator>
      <dc:date>2022-09-29T12:48:19Z</dc:date>
    </item>
    <item>
      <title>Re: Config SJA1105ELY</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Config-SJA1105ELY/m-p/1533344#M15442</link>
      <description>&lt;P&gt;Hi Lukas,&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you tell me what HW are you using exactly?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And also - assuming you are using the python tools to generate the configuration - can you provide the script you used?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 11:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Config-SJA1105ELY/m-p/1533344#M15442</guid>
      <dc:creator>kaden</dc:creator>
      <dc:date>2022-10-06T11:13:17Z</dc:date>
    </item>
  </channel>
</rss>