<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: SC18IM704PWJ GPIO6</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1510919#M15034</link>
    <description>&lt;P&gt;I am trying to connect the bridge to a half duplex UART (one wire arrangement),&lt;/P&gt;&lt;P&gt;I was thinking to activate through one of the I/O a one shot signal to control an external tri-state output buffer of the TX to enable Tx only when master on the UART expecting returned message. i was not sure if it can be done with the help of I2C on/off command&lt;/P&gt;</description>
    <pubDate>Wed, 24 Aug 2022 12:22:39 GMT</pubDate>
    <dc:creator>egershon</dc:creator>
    <dc:date>2022-08-24T12:22:39Z</dc:date>
    <item>
      <title>SC18IM704PWJ GPIO6</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1474084#M14356</link>
      <description>&lt;P&gt;The datasheet says the following:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="gpio6.PNG" style="width: 821px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183384i3F09CDB9503D2E9B/image-size/large?v=v2&amp;amp;px=999" role="button" title="gpio6.PNG" alt="gpio6.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So does that mean that when making a design that uses the SC18, the GPIO6 must have a pull-up resistor to it?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 05:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1474084#M14356</guid>
      <dc:creator>jj100126</dc:creator>
      <dc:date>2022-06-15T05:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IM704PWJ GPIO6</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1475120#M14371</link>
      <description>&lt;P&gt;Hello Joshua,&lt;/P&gt;
&lt;P&gt;Yes, the GPIO6 must have a pull-up resistor to ensure proper boot.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 07:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1475120#M14371</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-06-16T07:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IM704PWJ GPIO6</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1484410#M14544</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'd like to know why the SC18 in the evaluation board boots up even though there's no pull-up resistor on its GPIO6?&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="serial interface.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185539iC2636CD1CD678F3E/image-size/large?v=v2&amp;amp;px=999" role="button" title="serial interface.PNG" alt="serial interface.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jul 2022 06:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1484410#M14544</guid>
      <dc:creator>jj100126</dc:creator>
      <dc:date>2022-07-05T06:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IM704PWJ GPIO6</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1510919#M15034</link>
      <description>&lt;P&gt;I am trying to connect the bridge to a half duplex UART (one wire arrangement),&lt;/P&gt;&lt;P&gt;I was thinking to activate through one of the I/O a one shot signal to control an external tri-state output buffer of the TX to enable Tx only when master on the UART expecting returned message. i was not sure if it can be done with the help of I2C on/off command&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 12:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM704PWJ-GPIO6/m-p/1510919#M15034</guid>
      <dc:creator>egershon</dc:creator>
      <dc:date>2022-08-24T12:22:39Z</dc:date>
    </item>
  </channel>
</rss>