<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: LIN2.1 &amp;amp; SAE J2602</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/1509934#M15013</link>
    <description>&lt;P&gt;&lt;SPAN&gt;The SAE J2602 LIN specification is more restrictive compared to the LIN 2.x specification with regard to the following items: (1) the baud rate is limited to 10.417Kbps (compared to 20Kbps); (2) slave-to-slave communication is not allowed; (3) event triggered frames are not allowed; and, (4) EMI and ESD specs are more stringent.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 06:30:37 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-08-23T06:30:37Z</dc:date>
    <item>
      <title>LIN2.1 &amp; SAE J2602</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/1509869#M15012</link>
      <description>&lt;P&gt;The customer uses TJA1021 and uses Lin communication before. now use SAE J2602 protocol, does the software and hardware need to be changed, especially if the software changes greatly?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 04:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/1509869#M15012</guid>
      <dc:creator>jackyjiang20220620</dc:creator>
      <dc:date>2022-08-23T04:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: LIN2.1 &amp; SAE J2602</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/1509934#M15013</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The SAE J2602 LIN specification is more restrictive compared to the LIN 2.x specification with regard to the following items: (1) the baud rate is limited to 10.417Kbps (compared to 20Kbps); (2) slave-to-slave communication is not allowed; (3) event triggered frames are not allowed; and, (4) EMI and ESD specs are more stringent.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 06:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/1509934#M15013</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-08-23T06:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: LIN2.1 &amp; SAE J2602</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/2120386#M29054</link>
      <description>Hello, can you please suggest which RTM file can be used for this implementation in s32 v3.4 and if the SDK files also need the upgrade for this implementation</description>
      <pubDate>Fri, 20 Jun 2025 22:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LIN2-1-amp-SAE-J2602/m-p/2120386#M29054</guid>
      <dc:creator>mohit51099</dc:creator>
      <dc:date>2025-06-20T22:44:26Z</dc:date>
    </item>
  </channel>
</rss>