<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CodeWarrior USB Tap connector pitch in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-Tap-connector-pitch/m-p/1483309#M14522</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.&lt;/P&gt;
&lt;P&gt;pls select the right male 14 pin connector with 100 mil pitch.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Jul 2022 08:03:27 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2022-07-01T08:03:27Z</dc:date>
    <item>
      <title>CodeWarrior USB Tap connector pitch</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-Tap-connector-pitch/m-p/1482889#M14512</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I am designing a PCB and I want to include a 14-pin header to connect directly to CodeWarrior USB Tap. I can't seem to find any information regarding the connector pitch. Any help is appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jun 2022 15:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-Tap-connector-pitch/m-p/1482889#M14512</guid>
      <dc:creator>WO1</dc:creator>
      <dc:date>2022-06-30T15:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB Tap connector pitch</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-Tap-connector-pitch/m-p/1483309#M14522</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.&lt;/P&gt;
&lt;P&gt;pls select the right male 14 pin connector with 100 mil pitch.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 08:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-Tap-connector-pitch/m-p/1483309#M14522</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2022-07-01T08:03:27Z</dc:date>
    </item>
  </channel>
</rss>